This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368到底支不支持OTG功能?实际情况又是怎么样。。。



大家好:

        想问下,DM368这块芯片,当我的内核驱动和硬件电路都满足OTG功能要求时【即支持5V给外部供电,USB_ID线由外部设备触发】,到底支不支持OTG功能?我所说的OTG功能,要求如下:

       (1)  开机,内核起来,我插入一个USB CAMERA从设备,DM368能否正常识别?些时DM368当作主机设备HOST.

       (2)  再开机,使用同一个内核起来,我将DM368连接至PC机电脑?【注:连接电缆,已将USB_ID置于1高电平或悬空,即DM368工作于SLAVE模式】,PC机端,能否识别这个DM368的gadget驱动生成从设备,一般情况下,是g_file_storage.ko? modprobe g_file_storage.ko file=/dev/mmcblk0p2 stall=0 removable=1

       另外,想问一下:

       (1) 当工作于OTG模式时,低层驱动,根据什么检测设备插入?是否,此时,才去读USB_ID管脚,进而根据是HOST还是SLAVE,加载不同驱动或驱动的不同功能模块?

      (2) 当配置内核为OTG模式时,开机不接外部设备-USB_id悬空,DM368工作于OTG的哪一种模式?如果工作于从机模式,此时另一个USB从设备插入,将USB_ID管脚拉低?此时,DM368,能否由OTG的从模式,转换为OTG的主模式呢?

      先谢谢了~~

     感叹一下,DM368是否太老了。。。整个OTG功能都挺麻烦的。