This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI C6455 DSP芯片 GPIO 复用管脚问题



TI C6455 DSP芯片使用中有个问题,需请教专家指点下:
C6455 GPIO管脚部分为复用管脚,不仅是GPIO,还具有其他作用,
手册上显示GPIO 2是UTOPIA/PCI/GPIO复用,请教下如何才能使这个复用管脚工作为GPIO管脚呢
手册上说是通过device configration section部分来配置管脚状态,使用AEA0-AEA15上下拉来决定复用管脚功能
其他GP0/GP3等管脚的配置方法倒是找到了,但是我找遍了器件手册也没有发现关于GPIO2管脚的配置.

  • 在数据手册第37页上有描述,
    When the UTOPIA peripheral is disabled [UTOPIA_EN (AEA12 pin) = 0],these pins are PCI (if PCI_EN = 1) or GPIO (if PCI_EN = 0) pins (GP[15:12, 2]).
    所以通过设置AEA12=0, PCI_EN=0来使能GP2。