1.它使用TPS65218作为PMIC,按照《Powering the AM335x_AM437x with TPS65218》的推荐做法,应该用DCDC6的输出提供1.8V,供应SOC的VDDS_RTC管脚。
2。但实际上,GPEVM使用TPS78101来取代DCDC6的输出。
并且TPS78101的供电取用的是TPS65218的SYS_BU,手册上指出这个引脚是不推荐挂负载的!
3.如果按照推荐的做法,则可以实现在系统断电后,DCDC5与DCDC6依然正常工作,从而保证SOC的RTC依然正常工作。不过现在GPEVM的接法似乎就不能保证RTC依然可以正常工作了。
4.我想GPEVM是留了余地的,如果真的想实现上述功能,就把DCDC6输出处那个预留的焊盘上焊接0欧电阻,同时去掉TPS78101输入线上的0欧电阻。我这样的猜测是正确的吗?
5.如果上述理解是正确的,还有一个问题,为什么此处GPEVM要这样折腾?直接按推荐的做法不是很好吗?StarterKit就很老实