This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于am4378的GPEVM原理图上对VDDS_RTC供电的疑问

Other Parts Discussed in Thread: TPS65218

1.它使用TPS65218作为PMIC,按照《Powering the AM335x_AM437x with TPS65218》的推荐做法,应该用DCDC6的输出提供1.8V,供应SOC的VDDS_RTC管脚。

2。但实际上,GPEVM使用TPS78101来取代DCDC6的输出。

并且TPS78101的供电取用的是TPS65218的SYS_BU,手册上指出这个引脚是不推荐挂负载的!

3.如果按照推荐的做法,则可以实现在系统断电后,DCDC5与DCDC6依然正常工作,从而保证SOC的RTC依然正常工作。不过现在GPEVM的接法似乎就不能保证RTC依然可以正常工作了。

4.我想GPEVM是留了余地的,如果真的想实现上述功能,就把DCDC6输出处那个预留的焊盘上焊接0欧电阻,同时去掉TPS78101输入线上的0欧电阻。我这样的猜测是正确的吗?

5.如果上述理解是正确的,还有一个问题,为什么此处GPEVM要这样折腾?直接按推荐的做法不是很好吗?StarterKit就很老实

  • GPEVM这样做应该是考虑到TPS65218 CC引脚输入功率有限,DCDC5和DCDC6在电池供电时的输入电压范围是2.2-3.3V,DCDC5和DCDC6分别输出小于10uA和10uA电流的情况下,支持高达1Kohm的原阻抗+串联阻抗,如果负载和串联阻抗大于这个值,纽扣电池可能无法及时补充CC电容和SYS_BU电容上的能量,造成DCDC5和DCDC6因为SYS_BU引脚上电压太低而无法调节电压。而TPS78101是超低功耗LDO,输出150mA电流时,最低压降200mV,使得输出1.8V电压更加稳定。

  • 感谢您的分析!

    我之前一直有个误解,认为在系统断电的情况下,TPS78101是不能正常工作的。但其实它的输入SYS_BU在有电池的情形下,应该是有正常输出的。