This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

紧急求助,DM385 SDK 安装

Other Parts Discussed in Thread: IPNC-RDK-CSK

大家好,

       最近从供应商获得DM385的SDK,IPNC_RDK_V3.8.0-Linux-x86-Install.bin,安装出现如下问题

root@ubuntu:/mnt/hgfs/ubuntu104# ./IPNC_RDK_V3.8.0-Linux-x86-Install.bin
application-specific initialization failed: bad end of central directory record
%

报错initialization failed: bad end of central directory record,重新下载解压依然报错

    从官网下载IPNC-RDK-CSK-3.9.1-Linux-x86-Install.bin,安装报错

root@ubuntu:/mnt/hgfs/ubuntu104# chmod a+x IPNC-RDK-CSK-3.9.1-Linux-x86-Install.bin
root@ubuntu:/mnt/hgfs/ubuntu104# ./IPNC-RDK-CSK-3.9.1-Linux-x86-Install.bin
bash: ./IPNC-RDK-CSK-3.9.1-Linux-x86-Install.bin: cannot execute binary file

我的liunx是ubuntu-10.04-desktop-i386,请问以上失败是什么原因呢,我只要安装一种就可以了