大家好,
最近从供应商获得DM385的SDK,IPNC_RDK_V3.8.0-Linux-x86-Install.bin,安装出现如下问题
root@ubuntu:/mnt/hgfs/ubuntu104# ./IPNC_RDK_V3.8.0-Linux-x86-Install.bin
application-specific initialization failed: bad end of central directory record
%
报错initialization failed: bad end of central directory record,重新下载解压依然报错
从官网下载IPNC-RDK-CSK-3.9.1-Linux-x86-Install.bin,安装报错
root@ubuntu:/mnt/hgfs/ubuntu104# chmod a+x IPNC-RDK-CSK-3.9.1-Linux-x86-Install.bin
root@ubuntu:/mnt/hgfs/ubuntu104# ./IPNC-RDK-CSK-3.9.1-Linux-x86-Install.bin
bash: ./IPNC-RDK-CSK-3.9.1-Linux-x86-Install.bin: cannot execute binary file
我的liunx是ubuntu-10.04-desktop-i386,请问以上失败是什么原因呢,我只要安装一种就可以了