我安装的是CCS5.5,使用的编译器c6000_7.4.14。安装起后能正常编译;
过了一段时间编译工程提示,编译器提示版本不对"Description Resource Path Location TypeThis project was created using a version of compiler that is not currently installed: 7.4.14 [C6000]. Please install the compiler of this version, or migrate the project to one of the available compiler versions by adjusting project properties. NonOS_GPIO_KEY properties Problems“。
卸载编译器,重新安装编译器,可以使用了。这个问题发生了两次,都是重新安装编译器。
后来打开CCS5.5属性设置中,里面有一个选项:CG_TOOL_ROOT,路径丢失了,想直接修改路径,不用在重新安装编译器。结果发现添加不了。提示CG_TOOL_ROOT已有该项,想删除该项,可是又没有删除按键的地方? 很苦闷!!!!!!!!!!!!!!!!!!!!!
请问,该如何添加CG_TOOL_ROOT变量的路径? (提示:我们的PC机环境是XP系统, 我目前已经安装了一个CC3.3。)