This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

编译器路径总是丢了,请教如何处理



        我安装的是CCS5.5,使用的编译器c6000_7.4.14。安装起后能正常编译;

       过了一段时间编译工程提示,编译器提示版本不对"Description Resource Path Location TypeThis project was created using a version of compiler that is not currently installed: 7.4.14 [C6000]. Please install the compiler of this version, or migrate the project to one of the available compiler versions by adjusting project properties. NonOS_GPIO_KEY properties Problems“。

         卸载编译器,重新安装编译器,可以使用了。这个问题发生了两次,都是重新安装编译器。

        后来打开CCS5.5属性设置中,里面有一个选项:CG_TOOL_ROOT,路径丢失了,想直接修改路径,不用在重新安装编译器。结果发现添加不了。提示CG_TOOL_ROOT已有该项,想删除该项,可是又没有删除按键的地方? 很苦闷!!!!!!!!!!!!!!!!!!!!!

        请问,该如何添加CG_TOOL_ROOT变量的路径?  (提示:我们的PC机环境是XP系统, 我目前已经安装了一个CC3.3。)