This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Sitara AM3517

Other Parts Discussed in Thread: AM3517

Dear all.

      我在用Flash V1.6烧写xloader,uboot,或者是erase all AM3517主板时,总是提示 

Operation FAILED (Status malformed response (1 bytes))

Elapsed time: 0:00.000

 

Console program failed, exit code: 3

退出代码3:什么意思呢?通常是什么原因引起的?

以下是我调试过程中的提示信息,烦请大虾帮助分析一下。不甚感激。

-stdout

-omap 3

-no_force_package_alignment

-com 1

-t 60

-p CUSTOM_AM35XX_BOARD

-2

chip_erase NANDINFO1BITBOOT 0

Leaving parameter file:temp_script.txt

@temp_script.txt

Looking for device (omap com1)

Please turn off device, then turn it on again

Awaiting ASIC id

Awaiting ASIC id

AsicId items 04

AsicId id 01 05 01 34 30 07 58

AsicId secure_mode 13 02 01 00

AsicId public_id 12 15 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

AsicId root_key_hash 14 15 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

Searching 2nd for: CUSTOM_AM35XX_BOARD 343007 58 GP

Loading second file Targets\2nd-Downloaders\dnld_startup_omap3_gp_1g.2nd

Entering parameter file:omapflash2nd.txt at line: 7

-pheriphalboot_reopen

Reading board configuration file Targets\Configurations\configuration_custom_am35xx.txt

Reading definition file .\targets\definitions\definitions_omap3.txt

-board_config Targets\Configurations\configuration_custom_am35xx.txt

Leaving parameter file:omapflash2nd.txt

Sending size of second file (0x00006804 bytes)

Transferring second file to target (0x6804 bytes)

Closing boot connection

Found device (omap com1)

Waiting for 2nd

Found 2nd

Looking for a driver for 'NANDINFO1BITBOOT'

chip_driver NANDINFO1BITBOOT Targets\Flash-Drivers\nand_onfi_16bit_8bit.bin gpmc 0x6E000000 cs 0 address 0x30000000 bberase 0 onfi 0 bpp 2048 sbpp 64 ppb 64 bpl 1024 l 1 acv 0x22 f 0x0018 eTxp...

Downloading driver

Downloading 'Targets\Flash-Drivers\nand_onfi_16bit_8bit.bin'

 

Sending data (41008 bytes) :::::::::::::::..... [32764]

Sending data (41008 bytes) :::::::::::::::::::: [41008]

Sending data (41008 bytes) :::::::::::::::::::: [41008]

Download failed (final data response error): Status malformed response (1 bytes)

Elapsed time: 0:04.594 (10252 bytes/s)

Operation FAILED (Status malformed response (1 bytes))

Elapsed time: 0:00.000

 

Console program failed, exit code: 3