This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM320DM648的相关硬件设置



你好专家,请教几个硬件设计的问题,现在我们的设计遇到一个问题,就是器件的的正常上电加载会有不成功的情况出现,现在有几个问题想跟你们确认,

目前我们的BOOT模式是SPI启动,

你好专家,请教几个硬件设计的问题,现在我们的设计遇到一个问题,就是器件的的正常上电加载程序会有不成功的情况出现,现在有几个问题想跟你们确认,可能会有1%的不成功几率,

目前我们的BOOT模式是SPI启动,外接SPI FLASH,

1:NMI PIN设置,为什么DM642设置为高,但是在DM648中我将其上拉为高,RBL载入UBL的时候是可以的,但是UBL在加载应用程序时,不能进行下去,一定要我把NMI设置为下拉时UBL开可以加载应用程序成功,

2:C1 PIN规格书要求连接200欧姆电阻下拉到地,C2 PIN规格书要求为200欧姆电阻上拉到1.8V电源,Y12 PIN要求20欧姆电子上拉到3.3V,W12 PIN要求40欧姆电阻下来到地,但是开发板上的电阻规格都240欧姆,到底哪个是正确的规格,

3:SGMII接口的时钟输入管脚AB11,AC1之间规格书说内部已经包含了一个100欧姆的匹配电阻,但是参考设计上靠近管脚还有一个100欧姆的匹配电阻,请问这个电阻是否需要,规格书要求加入SGMII不使用,AB11 PIN需要短路到地,AC11需要短路到1.2V电源,请问是否需要,加入没有将他们连接到电源和地,会有什么样的影响,

4:个别设备还会出现CLKIN2输入信号正常但是DDR2的差分时钟没有信号输出的情况出现,整个器件工作不正常,有的将JTAG,的TCK下拉1K电阻会恢复正常,有的将SGMII接口的时钟输入信号去掉也会恢复正常,请问之间有逻辑关系吗,

DM648_bug.pdf