This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

some question about the refernece design "3D Machine Vision Reference Design Based on AM572x With DLP Structured Ligh"



1  What is the distance when the reference design reaches 30um--40um accuracy?

2 From the capture to the point cloud calculation out ,  it need 4.8s, if the deletion of "patern sorting" and only quickly calculate the rectangle long, wide, high, whether the opportunity to do within 1s?

3 The first phase of the current run in the CPU, the performance can not meet the needs of the factory, when is the second stage (DSP)   to be completed?