This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678调试发现waiting for ge rx interrupt timeout!求解



自己根据开发板设计的板卡,两片DSP,一片phy,一片16端口sgmii switch的bcm5396芯片。 两片dsp的sgmii 0都结在bcm5396上,phy芯片是88e1111,也通过sgmii接到bcm上 phy芯片的配置是 自协商,1000M fullduplex,bcm5396暂不用配置。例程采用网上的k1程序,dsp上的ge内部回环测试已经测试通过,现测试外部fifo回环的时候出现附件里的情况。参考时钟156.25m,passclk是100m,ethernet mode是1000m fullduplex,ge Port connection是0-sgmii connect;1-not used;两个dsp互为source和dest地址。 根据附件有几个问题: 1.waiting for ge rx interrupt timeout是为什么? 2.rxgoodframes 和 txgoodframes不同,发的少,收的多? 3.程序在打印print_ge_statistics时只打印到了statsb.netoctets,然后就没有了。啥原因,多谢