如上图所示,DM368的1.8V(上)和3.3V(下)上电时序,不知道为什么在1.8V上电后,3.3V未上电前,3.3V会被逐渐拉高到1.8V左右。
做过测试,完全断开DM368的3.3V输入,DM368的几个3.3V供电输入端也会有1.8V左右的电平,这排除了3.3V端的1.8V电平是DM368以外的器件串进来的。
那么,请问这种情况对DM368来说正常吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如上图所示,DM368的1.8V(上)和3.3V(下)上电时序,不知道为什么在1.8V上电后,3.3V未上电前,3.3V会被逐渐拉高到1.8V左右。
做过测试,完全断开DM368的3.3V输入,DM368的几个3.3V供电输入端也会有1.8V左右的电平,这排除了3.3V端的1.8V电平是DM368以外的器件串进来的。
那么,请问这种情况对DM368来说正常吗?
会不会是368内部电路的问题?以前做别的IC也碰到过类似的问题,只不过没有关注这么细节,关注你的结论
测试:
断开DM368的3.3V供电,但继续给系统1.35V和1.8V供电,观察此时的系统端3.3V电压档是否有串入电压。
1. 1.8V端:1.797V; 3.3V端:1.723V。
2. 取下部分外设芯片。
1.8V端:1.786V; 3.3V端:1.734V。
3. 取下所有外设芯片。
1.8V端:1.786V; 3.3V端:1.733V。
4. 取下FB4(1.8V_VDDS)。
1.8V端:1.803V; 3.3V端:2.312V。
5. 取下FB3(3.3V_VDDS)。
1.8V端:1.801V; 3.3V端:0.512V。 3.3V_VDDS=0.745V; 1.8V_VDDS=0.591V。
6. 短路FB4
1.8V端:1.796V; 3.3V端:0.392V。 3.3V_VDDS=1.786V。
7. 擦除DM368上所有程序。
1.8V端:1.802V; 3.3V端:1.774V。
8. 取下FB7(1.8V_VDD_PLL),取下FB6(1.8V_VDD_MXI),取下L3(1.8V_VDD_DAC),取下FB19(1.8V_VDD_USB)。
1.8V端:1.802V; 3.3V端:1.776V。 1.8V_VDD_DAC=1.192V,其他3挡基本没有电压。
9. 取下FB1(1.8V_DDR)
1.8V端:1.803V; 3.3V端:1.776V。 1.8V_DDR=0.908V
10. 取下FB13(3.3V_VDD_USB),取下FB11(3.3V_NAND_VCC)。
1.8V端:1.803V; 3.3V端:1.776V。3.3V_VDD_USB=1.876V,3.3V_NAND_VCC=1.208V。
结论:
1. 2-3步测试基本排除了主板上外设的影响。
2. 4-6步测试定位到了VDDS档对阶梯电压产生的影响比较大。
3. 7步排除DM368烧写程序与否的影响。
4. 8-10步测试基本可以得到结论:VDDS对于阶梯电压产生的影响是最主要的,其他部分电源输入端都有不同程度的电压串入问题。