我在使用6678时,分别编写了两个核的应用程序,分别进行编译和运行正常。但是当把CORE0程序下载到核0,然后将core1程序下载到核1,时,造成CORE0运行不正常,本该正常打印的初始化信息没有打印,在while循环内打中断,出现下面的错误提示信息。
C66xx_0: Breakpoint Manager: Retrying with a AET breakpoint
C66xx_0: Trouble Setting Breakpoint with the Action "Remain Halted" at 0xc00c50e: (Error -1199 @ 0xC00C50E) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 5.1.232.0)
具体程序如下:
CORE0:
Uint32 CoreNum;
int int_send_flag = 0;
TSC_init();
CoreNum = CSL_chipReadReg (CSL_CHIP_DNUM);
if(CoreNum==0)
{
//初始化PLL
if (C6678_Pll_Init(PLATFORM_PLL1_PLLM_val)!= TRUE)
{
printf("PLL failed to initialize!!!!!!!!!!!!!!!!!!!!!!!!! \n" );
}
else
{
printf("PLL succeeded in initialization\n" );
}
C6678_Power_UpDomains();
C6678_Ecc_Enable();
if (C6678_Ddr3_Init(PLLM_DDR3,DDR3_TYPE)!= TRUE)//DDR初始化
{
printf("DDR3 failed to initialize!!!!!!!!!!!!!!!!!!!!!!!!! \n" );
}
else
{
printf("DDR3 succeeded in initialization! \n" );
}
}
C6678_TimeCounter_Enable();
// C6678_CoreInt_Init ();
// C6678_ChipInt_Init (0);
IPC_Interrupt_Init_ZZG();
// C6678_CoreInt_Set (91,5,Core0INT_ISR,NULL);
// C6678_IPC_Intc_HookUp(Core0INT_ISR,5);
memset((void *)0x81000000,0,1024);
memset((void *)0x82000000,0,1024);
memset((void *)0x83000000,0,1024);
memset((void *)0x84000000,0,1024);
memset((void *)0x85000000,0,1024);
memset((void *)0x86000000,0,1024);
{
int_send_flag = *(volatile int*)0x85000000;
if(int_send_flag == 1 )
{
*(volatile int *)(0x85000000) = 0;
WritebackCache((void *)0x85000000,512);
uiDoorbell_startTSC = _itoll(TSCH,TSCL);
DEVICE_REG32_W(IPCGR(1), 0);
// C6678_CoreInt_Manual_trigger(5);
// C6678_IPC_Intc_send(1,1);
}
TSC_delay_us(50);
}
{
gpCGEM_regs->INTMUX1 = CSL_GEM_IPC_LOCAL <<CSL_CGEM_INTMUX1_INTSEL5_SHIFT;//0;//
gpCGEM_regs->INTMUX2 = 0;
gpCGEM_regs->INTMUX3 = 0;//CSL_GEM_GPINT13 <<CSL_CGEM_INTMUX3_INTSEL13_SHIFT;
gpCGEM_regs->EVTCLR[0]= 0xFFFFFFFF;
gpCGEM_regs->EVTCLR[1]= 0xFFFFFFFF;
gpCGEM_regs->EVTCLR[2]= 0xFFFFFFFF;
gpCGEM_regs->EVTCLR[3]= 0xFFFFFFFF;
ICR = IFR;
IER = IER|(1<<5); ////INT5的中断
//IER = IER|(1<<13); //INT13的中断
ISTP = 0x800000;
TSR = TSR|1;
IER = IER|(1<<CSL_CHIP_IER_NMI_SHIFT);
{
volatile uint32_t read_ipcgr;
uiDoorbell_endTSC = _itoll(TSCH,TSCL);
//
read_ipcgr = DEVICE_REG32_R(IPCGR(0));
DEVICE_REG32_W(IPCAR(0), read_ipcgr);
// C6678_IPC_Intc_Clear();
printf("sync_time = %d\n",TimeDiffer_Start_End);
//int int_send_flag = 0;
//初始化DDR
// C6678_TimeCounter_Enable();
// C6678_Sem2_MultiCore_Syn();
//初始化inter_Core INT
// C6678_CoreInt_Init ();
// C6678_ChipInt_Init (0);
IPC_Interrupt_Init_ZZG();
// C6678_CoreInt_Set (91,5,Core1INT_ISR,NULL);
// C6678_IPC_Intc_HookUp(Core0INT_ISR,5);
{
TSC_delay_us(50);
}
}
{
gpCGEM_regs->INTMUX1 = CSL_GEM_IPC_LOCAL <<CSL_CGEM_INTMUX1_INTSEL5_SHIFT;//0;//
gpCGEM_regs->INTMUX2 = 0;
gpCGEM_regs->INTMUX3 = 0;//CSL_GEM_GPINT13 <<CSL_CGEM_INTMUX3_INTSEL13_SHIFT;
gpCGEM_regs->EVTCLR[0]= 0xFFFFFFFF;
gpCGEM_regs->EVTCLR[1]= 0xFFFFFFFF;
gpCGEM_regs->EVTCLR[2]= 0xFFFFFFFF;
gpCGEM_regs->EVTCLR[3]= 0xFFFFFFFF;
ICR = IFR;
IER = IER|(1<<5); ////INT4的中断
//IER = IER|(1<<13); //INT13的中断
ISTP = 0x800000;
TSR = TSR|1;
IER = IER|(1<<CSL_CHIP_IER_NMI_SHIFT);
{
volatile uint32_t read_ipcgr;
uiDoorbell_endTSC = _itoll(TSCH,TSCL);
//
read_ipcgr = DEVICE_REG32_R(IPCGR(1));
DEVICE_REG32_W(IPCAR(1), read_ipcgr);
// C6678_IPC_Intc_Clear();
printf("sync_time = %d\n",TimeDiffer_Start_End);
-stack 0x4000
{
/* Local L2, 0.5~1MB*/
VECTORS: o = 0x00800000 l = 0x00000200
LL2: o = 0x00800200 l = 0x0003FE00
LL2_RW_DATA: o = 0x00840000 l = 0x00040000
SL2: o = 0x0C000000 l = 0x00200000
/* External DDR3, upto 2GB per core */
DDR3: o = 0x80000000 l = 0x20000000
}
{
vecs > VECTORS
.cinit > SL2
.const > SL2
.switch > SL2
.stack > LL2
GROUP
{
.neardata
.rodata
.bss
} > LL2
.far > LL2
.fardata > LL2
.cio > LL2
.sysmem > LL2
.i2ceeprom > LL2
/*
QMSS_Data.linkingRAM1 > SL2
QMSS_Data.Descriptor_SL2 > SL2
PacketData.buffer_SL2 > SL2
QMSS_Data.Descriptor_LL2 > LL2
PacketData.buffer_LL2 > LL2
QMSS_Data.Descriptor_DDR > DDR3_RW_DATA
PacketData.buffer_DDR > DDR3_RW_DATA*/
}