This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678 两个核下载程序相互影响,及核间中断配置



我在使用6678时,分别编写了两个核的应用程序,分别进行编译和运行正常。但是当把CORE0程序下载到核0,然后将core1程序下载到核1,时,造成CORE0运行不正常,本该正常打印的初始化信息没有打印,在while循环内打中断,出现下面的错误提示信息。 

C66xx_0: Breakpoint Manager: Retrying with a AET breakpoint
C66xx_0: Trouble Setting Breakpoint with the Action "Remain Halted" at 0xc00c50e: (Error -1199 @ 0xC00C50E) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 5.1.232.0)

具体程序如下:

CORE0:

void main(void) {
 
 Uint32   CoreNum;
 int int_send_flag = 0;
 TSC_init();
 CoreNum = CSL_chipReadReg (CSL_CHIP_DNUM);
 if(CoreNum==0)
 {
  //初始化PLL
  if (C6678_Pll_Init(PLATFORM_PLL1_PLLM_val)!= TRUE)
  {
   printf("PLL failed to initialize!!!!!!!!!!!!!!!!!!!!!!!!! \n" );
  }
  else
  {
   printf("PLL succeeded in initialization\n" );
  }
  /**/
  C6678_Power_UpDomains();
  C6678_Ecc_Enable();
  //初始化DDR
  if (C6678_Ddr3_Init(PLLM_DDR3,DDR3_TYPE)!= TRUE)//DDR初始化
  {
   printf("DDR3 failed to initialize!!!!!!!!!!!!!!!!!!!!!!!!! \n" );
  }
  else
  {
   printf("DDR3 succeeded in initialization! \n" );
  }
 }
 C6678_TimeCounter_Enable();
// C6678_CoreInt_Init ();
// C6678_ChipInt_Init (0);
 IPC_Interrupt_Init_ZZG();
// C6678_CoreInt_Set (91,5,Core0INT_ISR,NULL);
// C6678_IPC_Intc_HookUp(Core0INT_ISR,5);
 memset((void *)0x80000000,0,1024);
 memset((void *)0x81000000,0,1024);
 memset((void *)0x82000000,0,1024);
 memset((void *)0x83000000,0,1024);
 memset((void *)0x84000000,0,1024);
 memset((void *)0x85000000,0,1024);
 memset((void *)0x86000000,0,1024);
    while(1)
    {
     InvalidCache((void *)0x85000000,1024);
     int_send_flag = *(volatile int*)0x85000000;
     if(int_send_flag == 1 )
        {
      *(volatile int *)(0x85000000) = 0;
      WritebackCache((void *)0x85000000,512);
   uiDoorbell_startTSC  = _itoll(TSCH,TSCL);
   DEVICE_REG32_W(IPCGR(1), 0);
//   C6678_CoreInt_Manual_trigger(5);
//   C6678_IPC_Intc_send(1,1);
        }
     TSC_delay_us(50);
    }
}
/*中断配置*/
void IPC_Interrupt_Init_ZZG(void)
{
 gpCGEM_regs->INTMUX1 =  CSL_GEM_IPC_LOCAL  <<CSL_CGEM_INTMUX1_INTSEL5_SHIFT;//0;//
 gpCGEM_regs->INTMUX2 =  0;
 gpCGEM_regs->INTMUX3 = 0;//CSL_GEM_GPINT13  <<CSL_CGEM_INTMUX3_INTSEL13_SHIFT;
 /*Clear all DSP core events,一共是4个寄存器控制这么多,清除中断事件*/
 gpCGEM_regs->EVTCLR[0]=  0xFFFFFFFF;
 gpCGEM_regs->EVTCLR[1]=  0xFFFFFFFF;
 gpCGEM_regs->EVTCLR[2]=  0xFFFFFFFF;
 gpCGEM_regs->EVTCLR[3]=  0xFFFFFFFF;
 ICR = IFR;
 IER = IER|(1<<5);  ////INT5的中断
 //IER = IER|(1<<13);  //INT13的中断
 ISTP = 0x800000;
 TSR = TSR|1;
 IER = IER|(1<<CSL_CHIP_IER_NMI_SHIFT);
}
/*中断服务*/
interrupt void Core0INT_ISR(void)
{
 volatile uint32_t read_ipcgr;
 uiDoorbell_endTSC = _itoll(TSCH,TSCL);
//
 read_ipcgr = DEVICE_REG32_R(IPCGR(0));
    DEVICE_REG32_W(IPCAR(0), read_ipcgr);
// C6678_IPC_Intc_Clear();
 TimeDiffer_Start_End  = uiDoorbell_endTSC - uiDoorbell_startTSC;
 printf("sync_time = %d\n",TimeDiffer_Start_End);
}
CORE1:
void main(void) {
 
 //int int_send_flag = 0;
    //初始化DDR
// C6678_TimeCounter_Enable();
// C6678_Sem2_MultiCore_Syn();
 //初始化inter_Core INT
// C6678_CoreInt_Init ();
// C6678_ChipInt_Init (0);
 IPC_Interrupt_Init_ZZG();
// C6678_CoreInt_Set (91,5,Core1INT_ISR,NULL);
// C6678_IPC_Intc_HookUp(Core0INT_ISR,5);
    while(1)
    {
     TSC_delay_us(50);
    }
}
中断配置部分:
void IPC_Interrupt_Init_ZZG(void)
{
 gpCGEM_regs->INTMUX1 =  CSL_GEM_IPC_LOCAL  <<CSL_CGEM_INTMUX1_INTSEL5_SHIFT;//0;//
 gpCGEM_regs->INTMUX2 =  0;
 gpCGEM_regs->INTMUX3 = 0;//CSL_GEM_GPINT13  <<CSL_CGEM_INTMUX3_INTSEL13_SHIFT;
 /*Clear all DSP core events,一共是4个寄存器控制这么多,清除中断事件*/
 gpCGEM_regs->EVTCLR[0]=  0xFFFFFFFF;
 gpCGEM_regs->EVTCLR[1]=  0xFFFFFFFF;
 gpCGEM_regs->EVTCLR[2]=  0xFFFFFFFF;
 gpCGEM_regs->EVTCLR[3]=  0xFFFFFFFF;
 ICR = IFR;
 IER = IER|(1<<5);  ////INT4的中断
 //IER = IER|(1<<13);  //INT13的中断
 ISTP = 0x800000;
 TSR = TSR|1;
 IER = IER|(1<<CSL_CHIP_IER_NMI_SHIFT);
}
/*中断服务*/
interrupt void Core1INT_ISR(void)
{
 volatile uint32_t read_ipcgr;
 uiDoorbell_endTSC = _itoll(TSCH,TSCL);
//
 read_ipcgr = DEVICE_REG32_R(IPCGR(1));
    DEVICE_REG32_W(IPCAR(1), read_ipcgr);
    DEVICE_REG32_W(IPCGR(0), 1);
    // C6678_IPC_Intc_Clear();
 TimeDiffer_Start_End  = uiDoorbell_endTSC - uiDoorbell_startTSC;
 printf("sync_time = %d\n",TimeDiffer_Start_End);
}
两个核的CMD文件相同,如下:
-heap  0x2000
-stack 0x4000
MEMORY
{
 /* Local L2, 0.5~1MB*/
 VECTORS:      o = 0x00800000  l = 0x00000200
 LL2:          o = 0x00800200  l = 0x0003FE00
 LL2_RW_DATA:  o = 0x00840000  l = 0x00040000
 /* Shared L2 2~4MB*/
 SL2:   o = 0x0C000000  l = 0x00200000  
 
 /* External DDR3, upto 2GB per core */
 DDR3:      o = 0x80000000  l = 0x20000000
}
SECTIONS
{
 vecs        >    VECTORS
 .text           >    SL2
 .cinit          >    SL2
 .const          >    SL2
 .switch         >    SL2
 .stack          >    LL2
 GROUP
 {
  .neardata
  .rodata
  .bss
 }   >    LL2
 .far            >    LL2
 .fardata        >    LL2
 .cio            >    LL2
 .sysmem         >    LL2
 .i2ceeprom       >    LL2
/*
 QMSS_Data.linkingRAM1   >  SL2
 QMSS_Data.Descriptor_SL2  >  SL2
 PacketData.buffer_SL2   >  SL2
 QMSS_Data.Descriptor_LL2  >  LL2
 PacketData.buffer_LL2   >  LL2
 QMSS_Data.Descriptor_DDR  >  DDR3_RW_DATA
 PacketData.buffer_DDR   >  DDR3_RW_DATA*/
 
}