我用6678开发板跑demo,就是image processing的例子,在CCS的console中打印信息都正确,下面是一部分打印信息:
MCSDK IMAGE PROCESSING DEMONSTRATION
QMSS successfully initialized
CPPI successfully initialized
PA successfully initialized
EVM in StaticIP mode at 192.168.2.100
Set IP address of PC to 192.168.2.101
PASS successfully initialized
Ethernet subsystem successfully initialized
Ethernet eventId : 48 and vectId (Interrupt) : 7
Registration of the EMAC Successful, waiting for link up ..
Network Added: If-1:192.168.2.100
Service Status: HTTP : Enabled : : 000
但是输入192.168.2.100,为什么打不开网页呢?