This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于SEED XDS560、CCS3.3、DM368



有个项目需要对DM368的uboot和ubl进行烧写,据说560仿真器和CCS3.3可以做到

但是不知道具体的步骤:

现在我这里有SEED XDS560USB、CCS3.3、DM368

同时有一份dm365的.gel文件,和一个烧写flash的.out文件

一步一步装完CCS3.3和XDS560的驱动之后,发现CCSSetup里面没有DM365和DM368

接着我选了ARM926ejs,倒是连接成功了。

把原来CCS里面默认的自带.gel文件换成我现有的dm365的.gel文件,我发现原来的那个.gel文件是tms470的设备文件

Load Program完成了,但是.out文件运行是失败的。

希望TI的专家通过上面的介绍能给我一些指点,比如CCS Setup里面如何选择目标设备?还需要装其他的配置文件么?