This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Capture Link功能特性



根据之前如何理解Link的帖子中说明的理解link的几个方面说明capture link功能特性如下

Property  Value 
Number of input queues  NA 
Number of output queues  4
CH from a VIP port can be sent to same or different output queue
Input Type  Interlaced / Progressive 
Input Data format  Configure up to 4 HW video ports 
YUV422 8/16-bit embedded sync mode
Non-mux / pixel mux mode
SD / HD capture 
Output Data format  YUV422/YUV420 (non-mux ONLY) 
Frame-rate control  @ input =NA
@ output = YES
Skip odd fields from D1 input on per CH basis, to reduce DDR BW in CIF DVR use-cases 
Channel enable/disable  NO 
Dynamic resolution change  @ input = NA
@ output = NO