This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6657 与fpga之间PCIE链路连接



我们自己做的板子上DSP与FPGA之间用的PCIE接口连接,DSP这端CCS上显示链路已经建立,状态到17,可是FPGA上抓取的信号显示link_up为低。

请问DSP这端链路显示已经建立,那么FPGA那边是不是也应给建立起来了。PCIE两端链路状态是不是应该是一致的,我们在FPGA上检测link_up信号为低,会不会只是没检测到呢?

  • 请问 DEBUG1[4]XMLH_LINK_UP是多少?FPGA PCIe那边初始化正确吗?
  • /* Setting PL_GEN2 */ //V2.0版本,2X、5Gbps,参考PCIe手册2-8页和3-133页
    memset (&setRegs, 0, sizeof(setRegs));
    gen2.numFts = 0x1F;
    gen2.dirSpd = 0x0; //0x1 5G 0X0 2.5G
    gen2.lnEn = 2;
    setRegs.gen2 = &gen2;

    我和你遇到了同样的问题,将gen2.dirSpd设置为0,将连接速率改为2.5G ,FPGA那边就显示linkup。

    虽然过了很久了,楼主应该也解决了,希望能给后来者一点点的参考经验