This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于OMAPL138上电1.8V被拉高的问题

Other Parts Discussed in Thread: OMAP-L138

OMAP-L138上电后1.8V被拉高到2.7V
按照勘误表上说,原因是3.3V上电时产生了漏电流,解决方法是在1.8V与地之间加电容或电阻,这两种方法都试了还是没有解决。
论坛上也有同样的问题,见贴http://www.deyisupport.com/question_answer/f/54/t/6758.aspx

说可能是reset信号问题,我按论坛上所说用镊子先短路reset与地,上电后在放开,1.8V仍然是被拉高的。
请问还有什么解决方案。
谢谢!
请尽快回复。