This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6713B的EDMA问题

Other Parts Discussed in Thread: TMS320C6713B

大家好。请教一个问题:我使用TMS320C6713B,程序中使用了EDMA,在调试中完全没有问题。将程序下载到FLASH内后,就有问题了。我有三块板子(板子一样,买的开发板),其中一块下程序进去可以运行。另外两块下程序进去后EDMA不进中断。大家有遇到过这种问题吗?或者应该从哪方面去查找原因。

我配置的代码如下:

#include <stdio.h>

#include <string.h>

#include <stdlib.h>

#include <math.h>

#include <ctype.h>

//CSL

#include <csl.h>

#include <csl_cache.h>

#include <csl_edma.h>

#include <csl_timer.h>

#include <csl_irq.h>

#include <csl_mcbsp.h>

#include <csl_edma.h>

……

short gBufferXmtPing[BUFFSIZE];  // Transmit PING buffer

short gBufferXmtPong[BUFFSIZE];  // Transmit PONG buffer

……

#define PING  0         

#define PONG  1

EDMA_Handle hEdmaXmt;            // EDMA channel handles

EDMA_Handle hEdmaReloadXmtPing;

EDMA_Handle hEdmaReloadXmtPong;

short gXmtChan;

unsigned char xmtdone = 0 ;

short pingORpong=PING;

/* Transmit side EDMA configuration */

EDMA_Config gEdmaConfigXmt = { 

    EDMA_FMKS(OPT, PRI, HIGH)          |  // Priority

    EDMA_FMKS(OPT, ESIZE, 16BIT)       |  // Element size

    EDMA_FMKS(OPT, 2DS, NO)            |  // 2 dimensional source?

    EDMA_FMKS(OPT, SUM, INC)           |  // Src update mode

    EDMA_FMKS(OPT, 2DD, NO)            |  // 2 dimensional dest

    EDMA_FMKS(OPT, DUM, NONE)          |  // Dest update mode

    EDMA_FMKS(OPT, TCINT, YES)         |  // Cause EDMA interrupt?

    EDMA_FMKS(OPT, TCC, OF(0))         |  // Transfer complete code

    EDMA_FMKS(OPT, LINK, YES)          |  // Enable link parameters?

    EDMA_FMKS(OPT, FS, NO),               // Use frame sync?

 

    (Uint32)&gBufferXmtPing,              // Src address

 

    EDMA_FMK (CNT, FRMCNT, NULL)       |  // Frame count

    EDMA_FMK (CNT, ELECNT, BUFFSIZE),     // Element count

   

    EDMA_FMKS(DST, DST, OF(0)),           // Dest address

 

    EDMA_FMKS(IDX, FRMIDX, DEFAULT)    |  // Frame index value

    EDMA_FMKS(IDX, ELEIDX, DEFAULT),      // Element index value

 

    EDMA_FMK (RLD, ELERLD, NULL)       |  // Reload element

    EDMA_FMK (RLD, LINK, NULL)            // Reload link

};

void initEdma(void)

{

    /* Configure transmit channel */

    hEdmaXmt = EDMA_open(EDMA_CHA_XEVT0, EDMA_OPEN_RESET);  // get hEdmaXmt handle and reset channel

    hEdmaReloadXmtPing = EDMA_allocTable(-1);               // get hEdmaReloadXmtPing handle

    hEdmaReloadXmtPong = EDMA_allocTable(-1);               // get hEdmaReloadXmtPong handle

   

    gEdmaConfigXmt.dst = MCBSP_getXmtAddr(hMcbsp0);         // set the desination address to McBSP1 DXR

       

    gXmtChan = EDMA_intAlloc(-1);                           // get an open TCC

    gEdmaConfigXmt.opt |= EDMA_FMK(OPT,TCC,gXmtChan);       // set TCC to gXmtChan

       

    EDMA_config(hEdmaXmt, &gEdmaConfigXmt);                 // then configure the registers

    EDMA_config(hEdmaReloadXmtPing, &gEdmaConfigXmt);       // and the reload forPing

   

    gEdmaConfigXmt.src = EDMA_SRC_OF(gBufferXmtPong);       // change the structure to have a source of Pong

    EDMA_config(hEdmaReloadXmtPong, &gEdmaConfigXmt);       // and configure the reload for Pong       

   

    EDMA_link(hEdmaXmt,hEdmaReloadXmtPong);                 // link the regs to Pong

    EDMA_link(hEdmaReloadXmtPong,hEdmaReloadXmtPing);       // link Pong to Ping

    EDMA_link(hEdmaReloadXmtPing,hEdmaReloadXmtPong);       // and link Ping to Pong   

       

    /* Enable interrupts in the EDMA controller */

    EDMA_intClear(gXmtChan);   

 

    EDMA_intEnable(gXmtChan);                               // enable EDMA interrupts (CIER)

 

    EDMA_enableChannel(hEdmaXmt);                           // enable EDMA channel

   

    /* Do a dummy write to generate the first McBSP transmit event */

    MCBSP_write(hMcbsp0, 0);

}

/* McBSP codec data channel configuration */

static MCBSP_Config mcbspCfg0 = {

        MCBSP_FMKS(SPCR, FREE, NO)              |

        MCBSP_FMKS(SPCR, SOFT, NO)              |

        MCBSP_FMKS(SPCR, FRST, YES)             |

        MCBSP_FMKS(SPCR, GRST, YES)             |

        MCBSP_FMKS(SPCR, XINTM, XRDY)           |

        MCBSP_FMKS(SPCR, XSYNCERR, NO)          |

        MCBSP_FMKS(SPCR, XRST, YES)             |

        MCBSP_FMKS(SPCR, DLB, OFF)              |

        MCBSP_FMKS(SPCR, RJUST, RZF)            |

        MCBSP_FMKS(SPCR, CLKSTP, DISABLE)       |

        MCBSP_FMKS(SPCR, DXENA, OFF)            |

        MCBSP_FMKS(SPCR, RINTM, RRDY)           |

        MCBSP_FMKS(SPCR, RSYNCERR, NO)          |

        MCBSP_FMKS(SPCR, RRST, YES),

 

        MCBSP_FMKS(RCR, RPHASE, SINGLE)         |

        MCBSP_FMKS(RCR, RFRLEN2, DEFAULT)       |

        MCBSP_FMKS(RCR, RWDLEN2, DEFAULT)       |

        MCBSP_FMKS(RCR, RCOMPAND, MSB)          |

        MCBSP_FMKS(RCR, RFIG, NO)               |

        MCBSP_FMKS(RCR, RDATDLY, 0BIT)          |

        MCBSP_FMKS(RCR, RFRLEN1, OF(1))         |

        MCBSP_FMKS(RCR, RWDLEN1, 16BIT)         |

        MCBSP_FMKS(RCR, RWDREVRS, DISABLE),

 

        MCBSP_FMKS(XCR, XPHASE, SINGLE)         |

        MCBSP_FMKS(XCR, XFRLEN2, DEFAULT)       |

        MCBSP_FMKS(XCR, XWDLEN2, DEFAULT)       |

        MCBSP_FMKS(XCR, XCOMPAND, MSB)          |

        MCBSP_FMKS(XCR, XFIG, NO)               |

        MCBSP_FMKS(XCR, XDATDLY, 0BIT)          |

        MCBSP_FMKS(XCR, XFRLEN1, OF(1))         |

        MCBSP_FMKS(XCR, XWDLEN1, 16BIT)         |

        MCBSP_FMKS(XCR, XWDREVRS, DISABLE),

       

        MCBSP_FMKS(SRGR, GSYNC, DEFAULT)        |

        MCBSP_FMKS(SRGR, CLKSP, DEFAULT)        |

        MCBSP_FMKS(SRGR, CLKSM, DEFAULT)        |

        MCBSP_FMKS(SRGR, FSGM, DEFAULT)         |

        MCBSP_FMKS(SRGR, FPER, DEFAULT)         |

        MCBSP_FMKS(SRGR, FWID, DEFAULT)         |

        MCBSP_FMKS(SRGR, CLKGDV, DEFAULT),

 

        MCBSP_MCR_DEFAULT,

        MCBSP_RCER_DEFAULT,

        MCBSP_XCER_DEFAULT,

 

        MCBSP_FMKS(PCR, XIOEN, SP)              |

        MCBSP_FMKS(PCR, RIOEN, SP)              |

        MCBSP_FMKS(PCR, FSXM, EXTERNAL)         |

        MCBSP_FMKS(PCR, FSRM, EXTERNAL)         |

        MCBSP_FMKS(PCR, CLKXM, INPUT)           |

        MCBSP_FMKS(PCR, CLKRM, INPUT)           |

        MCBSP_FMKS(PCR, CLKSSTAT, DEFAULT)      |

        MCBSP_FMKS(PCR, DXSTAT, DEFAULT)        |

        MCBSP_FMKS(PCR, FSXP, ACTIVEHIGH)       |

        MCBSP_FMKS(PCR, FSRP, ACTIVEHIGH)       |

        MCBSP_FMKS(PCR, CLKXP, FALLING)         |

        MCBSP_FMKS(PCR, CLKRP, RISING)

};

 

void initMcbsp0()

{

    /* Open the codec data McBSP */

    hMcbsp0 = MCBSP_open(MCBSP_DEV0, MCBSP_OPEN_RESET);

 

    /* Configure the codec to match the AIC23 data format */

    MCBSP_config(hMcbsp0, &mcbspCfg0);

 

    /* Start the McBSP running */

    MCBSP_start(hMcbsp0, MCBSP_XMIT_START | MCBSP_RCV_START |

        MCBSP_SRGR_START | MCBSP_SRGR_FRAMESYNC, 220);

}

void initMcbsp1()

{

……

}

 

void main(){

       CSL_init();                          /* initialize the CSL library */

       DEVCFG = 0x0;

       Init_PLL();                          /*initialize PLL*/

       Init_EMIF();                         /*initialize emif */

       for(i=0;i<BUFFSIZE;i++)

       {

              gBufferXmtPing[i] = 0 ;

              gBufferXmtPong[i] = 0 ;

       }

       initMcbsp0();

       initMcbsp1();

       ……                                           

       IRQ_globalDisable();                 /* Disable all interrupts        */

       initEdma();

       IER=1;                               /* Disable all interrupts except NMI   */

       IRQ_setVecs((void *)0x800);             /* point to the IRQ vector table */

      ICR = 0x0ffff ;

      IER |= 0x4133;                           /*enable EXINT4 EXINT5 TIME0 EDMA interrupt*/

      IRQ_globalEnable();                  /*enable all interrupts*/ 

       ……

       while(1)

       {

       ……

       }

}