大家好。请教一个问题:我使用TMS320C6713B,程序中使用了EDMA,在调试中完全没有问题。将程序下载到FLASH内后,就有问题了。我有三块板子(板子一样,买的开发板),其中一块下程序进去可以运行。另外两块下程序进去后EDMA不进中断。大家有遇到过这种问题吗?或者应该从哪方面去查找原因。
我配置的代码如下:
#include <stdio.h>
#include <string.h>
#include <stdlib.h>
#include <math.h>
#include <ctype.h>
//CSL
#include <csl.h>
#include <csl_cache.h>
#include <csl_edma.h>
#include <csl_timer.h>
#include <csl_irq.h>
#include <csl_mcbsp.h>
#include <csl_edma.h>
……
short gBufferXmtPing[BUFFSIZE]; // Transmit PING buffer
short gBufferXmtPong[BUFFSIZE]; // Transmit PONG buffer
……
#define PING 0
#define PONG 1
EDMA_Handle hEdmaXmt; // EDMA channel handles
EDMA_Handle hEdmaReloadXmtPing;
EDMA_Handle hEdmaReloadXmtPong;
short gXmtChan;
unsigned char xmtdone = 0 ;
short pingORpong=PING;
/* Transmit side EDMA configuration */
EDMA_Config gEdmaConfigXmt = {
EDMA_FMKS(OPT, PRI, HIGH) | // Priority
EDMA_FMKS(OPT, ESIZE, 16BIT) | // Element size
EDMA_FMKS(OPT, 2DS, NO) | // 2 dimensional source?
EDMA_FMKS(OPT, SUM, INC) | // Src update mode
EDMA_FMKS(OPT, 2DD, NO) | // 2 dimensional dest
EDMA_FMKS(OPT, DUM, NONE) | // Dest update mode
EDMA_FMKS(OPT, TCINT, YES) | // Cause EDMA interrupt?
EDMA_FMKS(OPT, TCC, OF(0)) | // Transfer complete code
EDMA_FMKS(OPT, LINK, YES) | // Enable link parameters?
EDMA_FMKS(OPT, FS, NO), // Use frame sync?
(Uint32)&gBufferXmtPing, // Src address
EDMA_FMK (CNT, FRMCNT, NULL) | // Frame count
EDMA_FMK (CNT, ELECNT, BUFFSIZE), // Element count
EDMA_FMKS(DST, DST, OF(0)), // Dest address
EDMA_FMKS(IDX, FRMIDX, DEFAULT) | // Frame index value
EDMA_FMKS(IDX, ELEIDX, DEFAULT), // Element index value
EDMA_FMK (RLD, ELERLD, NULL) | // Reload element
EDMA_FMK (RLD, LINK, NULL) // Reload link
};
void initEdma(void)
{
/* Configure transmit channel */
hEdmaXmt = EDMA_open(EDMA_CHA_XEVT0, EDMA_OPEN_RESET); // get hEdmaXmt handle and reset channel
hEdmaReloadXmtPing = EDMA_allocTable(-1); // get hEdmaReloadXmtPing handle
hEdmaReloadXmtPong = EDMA_allocTable(-1); // get hEdmaReloadXmtPong handle
gEdmaConfigXmt.dst = MCBSP_getXmtAddr(hMcbsp0); // set the desination address to McBSP1 DXR
gXmtChan = EDMA_intAlloc(-1); // get an open TCC
gEdmaConfigXmt.opt |= EDMA_FMK(OPT,TCC,gXmtChan); // set TCC to gXmtChan
EDMA_config(hEdmaXmt, &gEdmaConfigXmt); // then configure the registers
EDMA_config(hEdmaReloadXmtPing, &gEdmaConfigXmt); // and the reload forPing
gEdmaConfigXmt.src = EDMA_SRC_OF(gBufferXmtPong); // change the structure to have a source of Pong
EDMA_config(hEdmaReloadXmtPong, &gEdmaConfigXmt); // and configure the reload for Pong
EDMA_link(hEdmaXmt,hEdmaReloadXmtPong); // link the regs to Pong
EDMA_link(hEdmaReloadXmtPong,hEdmaReloadXmtPing); // link Pong to Ping
EDMA_link(hEdmaReloadXmtPing,hEdmaReloadXmtPong); // and link Ping to Pong
/* Enable interrupts in the EDMA controller */
EDMA_intClear(gXmtChan);
EDMA_intEnable(gXmtChan); // enable EDMA interrupts (CIER)
EDMA_enableChannel(hEdmaXmt); // enable EDMA channel
/* Do a dummy write to generate the first McBSP transmit event */
MCBSP_write(hMcbsp0, 0);
}
/* McBSP codec data channel configuration */
static MCBSP_Config mcbspCfg0 = {
MCBSP_FMKS(SPCR, FREE, NO) |
MCBSP_FMKS(SPCR, SOFT, NO) |
MCBSP_FMKS(SPCR, FRST, YES) |
MCBSP_FMKS(SPCR, GRST, YES) |
MCBSP_FMKS(SPCR, XINTM, XRDY) |
MCBSP_FMKS(SPCR, XSYNCERR, NO) |
MCBSP_FMKS(SPCR, XRST, YES) |
MCBSP_FMKS(SPCR, DLB, OFF) |
MCBSP_FMKS(SPCR, RJUST, RZF) |
MCBSP_FMKS(SPCR, CLKSTP, DISABLE) |
MCBSP_FMKS(SPCR, DXENA, OFF) |
MCBSP_FMKS(SPCR, RINTM, RRDY) |
MCBSP_FMKS(SPCR, RSYNCERR, NO) |
MCBSP_FMKS(SPCR, RRST, YES),
MCBSP_FMKS(RCR, RPHASE, SINGLE) |
MCBSP_FMKS(RCR, RFRLEN2, DEFAULT) |
MCBSP_FMKS(RCR, RWDLEN2, DEFAULT) |
MCBSP_FMKS(RCR, RCOMPAND, MSB) |
MCBSP_FMKS(RCR, RFIG, NO) |
MCBSP_FMKS(RCR, RDATDLY, 0BIT) |
MCBSP_FMKS(RCR, RFRLEN1, OF(1)) |
MCBSP_FMKS(RCR, RWDLEN1, 16BIT) |
MCBSP_FMKS(RCR, RWDREVRS, DISABLE),
MCBSP_FMKS(XCR, XPHASE, SINGLE) |
MCBSP_FMKS(XCR, XFRLEN2, DEFAULT) |
MCBSP_FMKS(XCR, XWDLEN2, DEFAULT) |
MCBSP_FMKS(XCR, XCOMPAND, MSB) |
MCBSP_FMKS(XCR, XFIG, NO) |
MCBSP_FMKS(XCR, XDATDLY, 0BIT) |
MCBSP_FMKS(XCR, XFRLEN1, OF(1)) |
MCBSP_FMKS(XCR, XWDLEN1, 16BIT) |
MCBSP_FMKS(XCR, XWDREVRS, DISABLE),
MCBSP_FMKS(SRGR, GSYNC, DEFAULT) |
MCBSP_FMKS(SRGR, CLKSP, DEFAULT) |
MCBSP_FMKS(SRGR, CLKSM, DEFAULT) |
MCBSP_FMKS(SRGR, FSGM, DEFAULT) |
MCBSP_FMKS(SRGR, FPER, DEFAULT) |
MCBSP_FMKS(SRGR, FWID, DEFAULT) |
MCBSP_FMKS(SRGR, CLKGDV, DEFAULT),
MCBSP_MCR_DEFAULT,
MCBSP_RCER_DEFAULT,
MCBSP_XCER_DEFAULT,
MCBSP_FMKS(PCR, XIOEN, SP) |
MCBSP_FMKS(PCR, RIOEN, SP) |
MCBSP_FMKS(PCR, FSXM, EXTERNAL) |
MCBSP_FMKS(PCR, FSRM, EXTERNAL) |
MCBSP_FMKS(PCR, CLKXM, INPUT) |
MCBSP_FMKS(PCR, CLKRM, INPUT) |
MCBSP_FMKS(PCR, CLKSSTAT, DEFAULT) |
MCBSP_FMKS(PCR, DXSTAT, DEFAULT) |
MCBSP_FMKS(PCR, FSXP, ACTIVEHIGH) |
MCBSP_FMKS(PCR, FSRP, ACTIVEHIGH) |
MCBSP_FMKS(PCR, CLKXP, FALLING) |
MCBSP_FMKS(PCR, CLKRP, RISING)
};
void initMcbsp0()
{
/* Open the codec data McBSP */
hMcbsp0 = MCBSP_open(MCBSP_DEV0, MCBSP_OPEN_RESET);
/* Configure the codec to match the AIC23 data format */
MCBSP_config(hMcbsp0, &mcbspCfg0);
/* Start the McBSP running */
MCBSP_start(hMcbsp0, MCBSP_XMIT_START | MCBSP_RCV_START |
MCBSP_SRGR_START | MCBSP_SRGR_FRAMESYNC, 220);
}
void initMcbsp1()
{
……
}
void main(){
CSL_init(); /* initialize the CSL library */
DEVCFG = 0x0;
Init_PLL(); /*initialize PLL*/
Init_EMIF(); /*initialize emif */
for(i=0;i<BUFFSIZE;i++)
{
gBufferXmtPing[i] = 0 ;
gBufferXmtPong[i] = 0 ;
}
initMcbsp0();
initMcbsp1();
……
IRQ_globalDisable(); /* Disable all interrupts */
initEdma();
IER=1; /* Disable all interrupts except NMI */
IRQ_setVecs((void *)0x800); /* point to the IRQ vector table */
ICR = 0x0ffff ;
IER |= 0x4133; /*enable EXINT4 EXINT5 TIME0 EDMA interrupt*/
IRQ_globalEnable(); /*enable all interrupts*/
……
while(1)
{
……
}
}