平台:C5515
操作系统:DSP/BIOS
IDE:CCS 6.0
当前程序运行正常,基本占满了片上的DARAM和SARAM,为了后续增加功能,需要使用外挂的SDRAM来运行程序。
step1.查看编译生成的.map文件,发现.text段最大,为0x000226c0字节。
step2.打开.tcf文件,将.text段从原来的SARAM改为SRAM,即SDRAM。
step3.在.ccxml文件中使用GEL文件。
GEL文件中只保留一个有效的函数
OnTargetConnect()
{
//GEL_Reset();
//Peripheral_Reset();
ProgramPLL_100MHz();
SDRAM_INIT();
GEL_TextOut("Target Connection Complete.\n");
}
调用的两个函数代码如下:
ProgramPLL_100MHz() {
int i;
GEL_TextOut("Configuring PLL (100.00 MHz).\n");
/* Enable clocks to all peripherals */
*(short *)PCGCR1@IO = 0x0;
*(short *)PCGCR2@IO = 0x0;
/* Bypass PLL */
*(short *)CCR2@IO = 0x0;
/* Set CLR_CNTL = 0 */
*(short *)CGCR1@IO = *(short *)CGCR1@IO & 0x7FFF;
*(short *)CGCR1@IO = 0x8BE8;
*(short *)CGCR2@IO = 0x8000;
*(short *)CGCR3@IO = 0x0806;
*(short *)CGCR4@IO = 0x0000;
/* Wait for PLL lock */
for(i=0;i<0x7fff;i++);
/* Switch to PLL clk */
*(short *)CCR2@IO = 0x1;
GEL_TextOut("PLL Init Done.\n");
}
/* mSDRAM = MT48H4M16LF-8 */
/* Timings based on EMIF clk = 100MHz */
SDRAM_INIT()
{
int i;
/* reset EMIF */
*(short *)PRCR@IO = 0x0002;
for(i=0;i<0xff;i++);
//enable SDRAM clock
*(short*)CLKCFGL@IO=0x0001;
/* enable word writes to EMIF regs */
*(short *)ESCR@IO = 0;
/* step 1 */
*(short *)SDTIMR1@IO = 0x4710;
*(short *)SDTIMR2@IO = 0x3911;
*(short *)SDSRETR@IO = 0x0007;
/* step 2 */
*(short *)SDRCR@IO = 0x04E3;
/* step 3 */
*(short *)SDCR1@IO = 0x4720;
*(short *)SDCR2@IO = 0x0001;
/* step 4 */
for(i=0;i<0xff;i++);
/* step 5 */
*(short *)SDRCR@IO = 0x061A;
GEL_TextOut("SDRAM Initialization Complete.\n");
}
step4.编译,在线调试功能正常。
step5.将编译生成的.out文件通过hex55.exe转换成.bin文件。所用的.cmd文件内容如下:
-boot -v5505 -serial8 -reg_config 0x1C1F,0x0 -reg_config 0x1C20,0x8BB4 -reg_config 0x1C21,0x8000 -reg_config 0x1C22,0x0806 -reg_config 0x1C23,0x0200 -reg_config 0x3000,0x0002 -delay 0x500 -reg_config 0x1C1F,0x1
-reg_config 0x1C05,0x0002 -delay 0x500 -reg_config 0x1c1e,0x0001 -reg_config 0x1c33,0x0000 -reg_config 0x1020,0x4710 -reg_config 0x1021,0x3911 -reg_config 0x103C,0x0007 -reg_config 0x100C,0x04E3 -reg_config 0x1008,0x4720 -reg_config 0x1009,0x0001 -delay 0x500 -reg_config 0x100C,0x061A -b -o EVM_Sample.bin EVM_Sample.out
即,在.cmd文件中实现GEL文件的两个函数的功能。
step6.烧录到SPI flash上,无法正常运行。
请问:上述操作是否正确?
如果不正确,怎样操作才能实现在脱机情况下,在SDRAM运行程序呢?