This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

816X EVM u-boot下NFS挂接文件系统出错



硬件平台是TI的DM816X/AM389X开发板,SD卡启动后,在Uboot下,通过TFTP可以下载内核到内存并运行,但是不能通过NFS挂接根文件系统,bootargs=noinitrd root=/dev/nfs nfsroot=172.16.114.24:/nfsdir/xxb/rootfs ip=172.16.114.180:172.16.114.24:172.16.114.1:255.255.255.0::eth0 off'   内核通过TFTP下载到内存后通过bootm命令启动内核,故障信息如下:

VFS: Unable to mount root fs via NFS, trying floppy.                            
VFS: Cannot open root device "nfs" or unknown-block(2,0)                        
Please append a correct "root=" boot option; here are the available partitions: 
1f00             128 mtdblock0 (driver?)                                        
1f01             128 mtdblock1 (driver?)                                        
1f02             512 mtdblock2 (driver?)                                        
1f03            2048 mtdblock3 (driver?)                                                                               
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)

请问可能是什么原因?NFS主机端自己可以挂载自己,kernel配置也检查了