This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6416 GPIO输出问题请教



   各位大神:

      目前在测试DSP C6416 跟FPGA之间直连GPIO管教GP8\GP9\GP10\GP11\GP12时,发现DSP将GP8/GP9/GP10/GP11/GP12配置为输出,

      且周期1s设置GP8/GP9/GP10/GP11/GP12管脚高低输出跳变,FPGA端检测不到GP8/GP9/GP10/GP11/GP12信号变化,具体测试设置方法如下红色字体描述,请各位高手指点,谢谢!!

      6416 GPIO管脚配置如下:

      #define GPEN   *(volatile Uint32*)0x01b00000

      #define GPDIR  *(volatile Uint32*)0x01b00004

      #define GPVAL  *(volatile Uint32*)0x01b00008

     GPEN  |= ((1 <<8) | (1 <<9) | (1 << 10)|(1<<11)|(1<<12));

      GPDIR |= ((1 <<8) | (1 <<9) | (1 << 10)|(1<<11)|(1<<12));

      延迟1S

       /*拉低管脚*/

      GPVAL &= 0xE0FF;

       延迟1S

      GPVAL |= 0x1F00;