This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好,请教个问题
在C6678 EVM中,UCD9222的一个VID连接C6678,用于动态调整电压CVDD,这点我能理解。
但是,UCD9222的另一个VID引脚连接到了FPGA,而UCD9222这个电压输出应该是给C6678提供的fixed电压VCC1V0的吧。
那么为什么还要把这个电压输出通道的VID连接到FPGA?FPGA通过VID对UCD9222的这个电压输出通道做了什么?是预留功能吗?把UCD9222这个通道的VID空接,行不行?
顺便问一下,有没有关于C6678的QQ讨论群,那样的话,讨论起来会更加方便一点
多谢大家了~~~
UCD9222可以同时给两个DSP提供可变核电压,因为EVM上只有一个DSP,还有一路是reserved。Fix 1V可以通过其它DC-DC如TPS54620来提供,不需要经过UCD.