This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678 EVM UCD9222

Other Parts Discussed in Thread: UCD9222, TPS54620

大家好,请教个问题

在C6678 EVM中,UCD9222的一个VID连接C6678,用于动态调整电压CVDD,这点我能理解。

但是,UCD9222的另一个VID引脚连接到了FPGA,而UCD9222这个电压输出应该是给C6678提供的fixed电压VCC1V0的吧。

那么为什么还要把这个电压输出通道的VID连接到FPGA?FPGA通过VID对UCD9222的这个电压输出通道做了什么?是预留功能吗?把UCD9222这个通道的VID空接,行不行?

顺便问一下,有没有关于C6678的QQ讨论群,那样的话,讨论起来会更加方便一点

多谢大家了~~~