This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6657 Booting from the SPI NOR



板子使用的自己的板子DSP6657,

确定器件和EVM的一模一样,都是N25Q032A,测试应用软件用的ALLEN Yin1 给的C6657双核测试程序,生成出来.out 通过转换工具生成.dat文件,但是加载进EVM6657 nor write 工程后,烧写进nor flash中后 ,重启上电连接仿真器还是在RBL中 并没有启动起来。查看示波器,spi clk 正常500khz。修改spi.map文件的mode在0和1模式下还有时钟频率分别在1G和800Mhz还是同样的无法正常启动。在生成.dat文件中 修改了51-> 00。麻烦ti工程师指点迷津,看论坛很多人都是按照同样的步骤 但是无法从spi flash启动!(用的应用软件和转换工具都是ti论坛上的,也都是按照步骤来的)。magic address 看到的都是0!