使用C6678使用自带的helloworld进行软件仿真时,遇到了如下错误:
[TMS320C66x_0] Invalid CIO command (255) in the CIO buffer at address (0xC3173C0) was not recognized. Please check the device and program memory maps.
[TMS320C66x_1] Invalid CIO command (255) in the CIO buffer at address (0xC3173C0) was not recognized. Please check the device and program memory maps.
.....
请问这是怎么回事?
下面是target设置和测试时的情况