测试模式为SRIO_DIGITAL_LOOPBACK
根据例程测试说明文档,程序先跑1×LaneA模式,这时候gpSRIO_regs->RIO_PLM[0].RIO_PLM_SP_PATH_CTL应该是256啊,为啥expressions观察到的是1024?
然后跑2×LaneAB模式,gpSRIO_regs->RIO_PLM[0].RIO_PLM_SP_PATH_CTL应该是513啊,为啥expression显示的是1025?
请大神帮忙解答一下
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
测试模式为SRIO_DIGITAL_LOOPBACK
根据例程测试说明文档,程序先跑1×LaneA模式,这时候gpSRIO_regs->RIO_PLM[0].RIO_PLM_SP_PATH_CTL应该是256啊,为啥expressions观察到的是1024?
然后跑2×LaneAB模式,gpSRIO_regs->RIO_PLM[0].RIO_PLM_SP_PATH_CTL应该是513啊,为啥expression显示的是1025?
请大神帮忙解答一下
hello,
请问有结果了吗?
1.今天看到一篇帖子https://e2echina.ti.com/question_answer/dsp_arm/c6000_multicore/f/53/t/4942,里面提到PER_SET_CNTL中的boot complete用来决定只读位是否可以改写。我看了一下程序,在尝试修改Path_config之前,boot complete位是0,但是Path_config仍然不能被修改。
2.自动测试到 2 x LaneAB模式时,PLM_SP(n)_PATH_CTL寄存器的值是1025,即configration4,Mode1。但是根据Table2-4,[configration4,Mode1]时,2x的port应
该是使用LaneCD,而不是LaneAB。请帮忙解释下,谢谢!