This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位大牛:
现在在做Nand/Nor Falsh Boot via IBL ,使用led程序来验证boot成败,遇到一些问题,特此请教。
1).先烧写Nand flash 程序还是先向EEPROM中烧写IBL,参考其他人的有不同的顺序,对boot有没有影响?
2).在eepromwriter_input.txt 中bus_addr=0x51,那no boot mode 下的SW5是不是应该是0 0 0 1,但好多参考上选择的0 0 0 0,这是不是有关联?
3).加载过i2cparam_0x51_c6678_le_0x500.out和 setConfig_C6678_main(), Run后 CIO窗口右下角也会出现 CIO waiting input,按回车(enter)后出现“Error: I2C timed out, reported at stage: Block at offset 64 ”,这是什么原因?
4). i2cConfig.gel 文件中已经修改nandBoot.bootFormat=ibl_BOOT_FORMAT_ELF.
5).得知IBL会使用到L2内存,已经修改CMD错开L2区域,这和第三个问题有关联吗?
问题较多,请重点回答第三个问题,谢谢。
第三个问题,我已解决。是加载顺序问题,需要先运行i2cpram_0x51_c6678_le_0x500.out,然后加载i2cConfig.gel,-->SetConfig_C6678_main()后
回车键,I2C table complete.
新问题:
1)明明是正确的LED程序,仿真器调试也正确,为何下载到NAND Flash中自启动不可以实现??
2)eepromwriter_input.txt 中bus_addr=0x51问题,导致SW5的 4号键是否应该是OFF????
3) 不管是EEPROM_writer还是NAND_writer 、NOR_writer, Load momory 窗口中start address 都是0x80000000吗?那各自的_input.txt中是否需要修改?是不是程序是借助于DDR的0x80000000中传输到eeprom,nand ,nor?
Canyu:
你好,我现在也在做FLASH烧写的调试。接触6678不久,有些问题想要请教,方便的话加我QQ:327023905谢谢。
额,还有,能提供一下你的LED程序吗
zhonghong zhang 您好
我现在遇上了和您一样的问题。6678通过IBL从Nand Flash可以单核启动,但是多核启动一直没有好的解决方法。我的8个核是同一个out文件,在里面通NUM核号来做区别。请问您有这方面的成功经验吗。是否方便分享,哪怕提供点方向也可以。不胜感激!