This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678评估板连不上CCS



刚拿到6678LE的评估板,CCS是5.1版本,系统是Xp,安装完光盘提供的驱动安装程序后。

在no boot 方式下,给板子上电。打开CCS5.1后,创建配置文件后(用的是XDS100v1),点击“Test connection”。出现如下错误提示:

this error is generated by TI's USCIF driver or utilities.

this value is '-151'(0xffffff69)

the title is 'SC_ERR_POD_OPEN'.

the explanaton is :

this utility failed to open the adapter for a custom emulator .

the adapter returned an error

[end]

请高手帮下忙,这是哪里出了问题?板子是新买的。

 

  • 6678LE是带XDS560V2 mezzeline card的版本,你确认你连得是XDS100?

    上电后到windows设备管理器里看看是否检测到TI emulator,如果没有,换台电脑试试。

  • 非常感谢你的回答,6678LE是带一个XDS560V2 mezzeline card,但是我是把它拆了下来。因为带上它也不能和CCS连接上。我用的是板子上集成的XDS100V1仿真器(在文档上说,如果不装XDS5602外部仿真,就会自动用的是内置XDS100V1)。在电脑里的管理器,确实看到了 USB deposit  。