AM3352 板子中
在spi的读写程序中,设定SPI频率为20MHz
实际示波器测量时钟则只有16MHz的频率
切换到40MHz
实际测量时钟则只有23MHz的频率
设备树中的SPI最大频率设置为48MHz
哪里变了我的SPI时钟速率???
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
AM3352 板子中
在spi的读写程序中,设定SPI频率为20MHz
实际示波器测量时钟则只有16MHz的频率
切换到40MHz
实际测量时钟则只有23MHz的频率
设备树中的SPI最大频率设置为48MHz
哪里变了我的SPI时钟速率???