This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SPI时钟的频率不等于设定频率问题

Other Parts Discussed in Thread: AM3352

AM3352 板子中

在spi的读写程序中,设定SPI频率为20MHz

实际示波器测量时钟则只有16MHz的频率

切换到40MHz

实际测量时钟则只有23MHz的频率

设备树中的SPI最大频率设置为48MHz

哪里变了我的SPI时钟速率???