This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678(PG2.0)pcie加载程序成功,但是无法自启动



1.首先我把boot mode设置成pcie boot模式,然后利用windriver扫描到pcie的ID号,并可以正常读写

2.然后 我根据TI提供的基于linux的pciedemo.c移植到windows下,然后将ddrinit_code和helloword_code生成的.out文件转换成的.h文件通过pcie成功烧写到6678里面,通过仿真器查看写入的值都正确,但是就是没运行!!

3.尝试另一种方法-------先利用仿真器load ddrinit_code,并运行后,然后用上位机通过pcie加载helloword_code,helloword运行成功。

我查资料发现PG1.0,需要IBL,IBL里面有一个自启动的过程。

我想问一下PG2.0,只利用RBL怎么自启动啊?或者说pcie加载到6678的程序怎么让它自动运行?

顺便问一下,ti是否能提供PG2.0的RBL源码?

期待您的回复!