This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

麻烦问一下,是否有6678 SPI启动材料



目前做6678就差最后一步了,启动问题,自己编写好的6678程序怎么烧写到SPI的NOR flash里呀,是不是直接烧写进去就可以上电直接启动呀,我目前的工程下载到片内和片外都能运行,初始化如下

KeyStone_common_CPU_init();
/*print device information.
Enable memory protection interrupts, EDC for MSMC RAM*/
KeyStone_common_device_init();

//enable exception handling
KeyStone_Exception_cfg(TRUE);

KeyStone_main_PLL_init(100, 10, 1);

UART_Interact_with_PC();

GPIO_init();

目前电路板设计是按照EVM设计的,只有SPI的NOR Flash,所以只能从SPI的NOR Flash里启动,我想问一下,按照上面的初始化,是不是直接烧写到SPI的NOR Flash就可以启动,不需要I2C的 EEPROM参与?

如果需要做成能够直接从SPI中启动的工程,还缺什么初始化吗?