This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

在SD卡建立am335x-evm-linux-06.01.00.08后放在BeagleBoard显示"Please Wait..."就卡住



大家好,

我目前跟这篇 e2echina.ti.com/.../158425 遇到一样的问题,

在SD卡建立am335x-evm-linux-06.01.00.08后放在BeagleBoard显示"Please Wait..."就卡住不再动了

请问有大神知道如何解决的方法吗?

  • 烧入bbb官方提供的镜像是否正常?

  • 是的。烧入BBB官方自己的合并没问题,但将Ti的SDK替换烧入后再放置BBB开机就会卡在Please wait。

  • 是自己基于SDK自己编译的吗?
  • 是的,打算在BBB上放置Ti AM335x SDK并启动6lowpan程序,

    目前我尝试了一下将/etc/init.d/weston移除后可以正常开机了。

    但不知道weston这个目录夹在这个SDK中重要吗?移除不知道会如何?

  • 在weston文件夹里有哪些内容?

    这个主要是用在UI

  • ini.d内的weston档案在这里,请查看:

    4478.weston.zip


    我是新手,其实不太懂这里面的内容为什么会造成AM335X无法正常运行的原因。

    再麻烦协助解答了,万分感谢。

  • 我方才照着这个帖子输出了weston.log

    显示如下:

    [01:54:10.456] event2 - Wired USB Keyboard Consumer Control: device is a keyboard
    [01:54:10.617] DRM: head 'HDMI-A-1' found, connector 31 is connected, EDID make 'ACI', model 'ASUS MX239', serial 'H2LMTJ026153'
    [01:54:10.618] Registered plugin API 'weston_drm_output_api_v1' of size 12
    [01:54:10.620] format 0x34325258 not supported by output HDMI-A-1
    [01:54:10.620] Failed to init output gl state
    [01:54:10.620] Enabling output "HDMI-A-1" failed.
    [01:54:10.620] Error: cannot enable output 'HDMI-A-1' without heads.
    [01:54:10.624] event0 - Wired USB Keyboard: device removed
    [01:54:10.653] event1 - Wired USB Keyboard System Control: device removed
    [01:54:10.682] event2 - Wired USB Keyboard Consumer Control: device removed

    请问这个[01:54:10.620] format 0x34325258 not supported by output HDMI-A-1
    不支持这个HDMI输出代码是0x34325258,我应该如何解决呢?

    我也有按照帖子中先Stop matrix-gui-2.0 & Weston再Start过,
    似乎也没有任何的反应及改变~

    另外我也有尝试使用内文所述weston --tty = 1指令:
    root@am335x-evm:/# weston --tty = 1
    Date: 2020-02-10 UTC
    [02:04:04.884] weston 5.0.0
    https://wayland.freedesktop.org
    Bug reports to: https://gitlab.freedesktop.org/wayland/weston/issues/
    Build: unknown (not built from git or tarball)
    [02:04:04.889] Command line: weston --tty = 1
    [02:04:04.890] OS: Linux, 4.19.59-g5f8c1c6121, #1 PREEMPT Sat Oct 19 17:17:25 UTC 2019, armv7l
    [02:04:04.893] Using config file '/etc//weston.ini'
    [02:04:04.896] Output repaint window is 7 ms maximum.
    [02:04:04.899] Loading module '/usr/lib/libweston-5/wayland-backend.so'
    [02:04:04.900] Failed to load module: /usr/lib/libweston-5/wayland-backend.so: cannot open shared object file: No such file or directory
    [02:04:04.901] fatal: failed to create compositor backend

    但因为我是新手刚接触,所以我不是很懂要如何排除。

  • weston 文件夹去掉后正常启动,hdmi有输出吗
  • 有的!若去掉了 Weston 后开机就会正常的显示 root@am335x-evm:

    尝试了好几天这个问题还是无法排除,

    目前只好暂时使用 Putty 询问 IP Address 方式先使用并测试了。

  • 应该街上鼠标和键盘就可以用了吧