大家好,
我目前跟这篇 e2echina.ti.com/.../158425 遇到一样的问题,
在SD卡建立am335x-evm-linux-06.01.00.08后放在BeagleBoard显示"Please Wait..."就卡住不再动了
请问有大神知道如何解决的方法吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好,
我目前跟这篇 e2echina.ti.com/.../158425 遇到一样的问题,
在SD卡建立am335x-evm-linux-06.01.00.08后放在BeagleBoard显示"Please Wait..."就卡住不再动了
请问有大神知道如何解决的方法吗?
我方才照着这个帖子输出了weston.log
显示如下:
[01:54:10.456] event2 - Wired USB Keyboard Consumer Control: device is a keyboard
[01:54:10.617] DRM: head 'HDMI-A-1' found, connector 31 is connected, EDID make 'ACI', model 'ASUS MX239', serial 'H2LMTJ026153'
[01:54:10.618] Registered plugin API 'weston_drm_output_api_v1' of size 12
[01:54:10.620] format 0x34325258 not supported by output HDMI-A-1
[01:54:10.620] Failed to init output gl state
[01:54:10.620] Enabling output "HDMI-A-1" failed.
[01:54:10.620] Error: cannot enable output 'HDMI-A-1' without heads.
[01:54:10.624] event0 - Wired USB Keyboard: device removed
[01:54:10.653] event1 - Wired USB Keyboard System Control: device removed
[01:54:10.682] event2 - Wired USB Keyboard Consumer Control: device removed
请问这个[01:54:10.620] format 0x34325258 not supported by output HDMI-A-1
不支持这个HDMI输出代码是0x34325258,我应该如何解决呢?
我也有按照帖子中先Stop matrix-gui-2.0 & Weston再Start过,
似乎也没有任何的反应及改变~
另外我也有尝试使用内文所述weston --tty = 1指令:
root@am335x-evm:/# weston --tty = 1
Date: 2020-02-10 UTC
[02:04:04.884] weston 5.0.0
https://wayland.freedesktop.org
Bug reports to: https://gitlab.freedesktop.org/wayland/weston/issues/
Build: unknown (not built from git or tarball)
[02:04:04.889] Command line: weston --tty = 1
[02:04:04.890] OS: Linux, 4.19.59-g5f8c1c6121, #1 PREEMPT Sat Oct 19 17:17:25 UTC 2019, armv7l
[02:04:04.893] Using config file '/etc//weston.ini'
[02:04:04.896] Output repaint window is 7 ms maximum.
[02:04:04.899] Loading module '/usr/lib/libweston-5/wayland-backend.so'
[02:04:04.900] Failed to load module: /usr/lib/libweston-5/wayland-backend.so: cannot open shared object file: No such file or directory
[02:04:04.901] fatal: failed to create compositor backend
但因为我是新手刚接触,所以我不是很懂要如何排除。