This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FPGA通过SRIO向6678DSP的DDR中写数,同时DSP还要读取DDR其他地址的数据造成SRIO阻塞



尊敬的TI工程师,请问FPGA通过SRIO向6678DSP的DDR中写数,同时DSP还要读写DDR其他地址的数据造成SRIO阻塞,有什么好的解决办法吗?

如果我dsp在srio传输的过程中不做DDR的写入操作就没有问题,但是我是实时系统,肯定还要用DDR的数据进行计算并将数据再次写入到其他的DDR段上。

我看了好多帖子了,问题还未解决,目前我做的尝试如下:

1、将SRIO的地址放入SRIO的RIO_PER_SET_CNTL寄存器中CBA_TRANS_PRI字设为000;

设置方式:CSL_SRIO_SetTransactionPriority(hSrioCSL,0);

2、将MDMAARBU(0x01841010)设为0x06070000,代表着UPRI=6,PRI=7;

    *(unsigned int *)(0x01841010)=0x06070000;

3、将MDMAARBX(0x08000280)设为0x00060000,代表着PRI=6;

    *(unsigned int *)(0x08000280)=0x00060000;

您可以帮忙看看我这设置的有没有问题,如果没有问题接下来还有什么其他调试思路,有帖子中说改变操作DDR3的时序(DDR3 Memory Controller for KeyStone Devices User's Guide)才能完全规避,请问这大概怎么操作?