This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Q: 如何在CCS v7里重新编译在Serial flash and boot utilities for OMAPL138软件包里基于CCS的Flash Writer工程文件?
A: 有时候客户用的flash和EVM板上的不一样,需要做适当的修改并进行重新编译。
软件包里的CCS工程是基于CCS 3.3的,在CCS v7里重新编译的步骤如下:
软件要求:
Serial flash and boot utilities for OMAPL138
Compiler CGTools 7.4x
第一步: 到CCS->Windows->Preferences,添加Compiler 7.4.x路径,如下图
第二步: 点击CCS->Project->Import Legacy CCSv3.3 projects…选择compiler 7.4 和the common root,如下图: