This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] 【FAQ】重新编译软件包里的工程文件



Q: 如何在CCS v7里重新编译在Serial flash and boot utilities for OMAPL138软件包里基于CCS的Flash Writer工程文件?

A: 有时候客户用的flash和EVM板上的不一样,需要做适当的修改并进行重新编译。

https://processors.wiki.ti.com/index.php/Serial_Boot_and_Flash_Loading_Utility_for_OMAP-L138#Modifications_for_Custom_Boards

软件包里的CCS工程是基于CCS 3.3的,在CCS v7里重新编译的步骤如下:        
软件要求:

Serial flash and boot utilities for OMAPL138

Compiler CGTools 7.4x

第一步: 到CCS->Windows->Preferences,添加Compiler 7.4.x路径,如下图

第二步: 点击CCS->Project->Import Legacy CCSv3.3 projects…选择compiler 7.4 和the common root,如下图: