This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于AM5728的EDMA

对于AM5728的EDMA该如何使用,参考了Documentation/devicetree/bindings/ti-edma.txt 和Documentation/devicetree/bindings/ti-dma-crossbar.txt文档设置了设备树,但好像对数据没任何影响,连续读取数据速度依然很慢

  • 请问使用的SDK版本是什么?EDMA是用于哪个接口上实现数据搬移的?相关配置代码贴出来一下。
  • 内核是4.9.65
    设备树配置如下:在应用层直接映射gpmc地址,读取数据,速度远达不到设备树约束的速度

    edma: edma@43300000 {
    compatible = "ti,edma3-tpcc";
    ti,hwmods = "tpcc";
    reg = <0x43300000 0x100000>;
    reg-names = "edma3_cc";
    interrupts = <GIC_SPI 361 IRQ_TYPE_LEVEL_HIGH>,
    <GIC_SPI 360 IRQ_TYPE_LEVEL_HIGH>,
    <GIC_SPI 359 IRQ_TYPE_LEVEL_HIGH>;
    interrupt-names = "edma3_ccint", "edma3_mperr",
    "edma3_ccerrint";
    dma-requests = <64>;
    #dma-cells = <2>;

    ti,tptcs = <&edma_tptc0 7>, <&edma_tptc1 0>;
    ti,edma-memcpy-channels = <20 21>;
    /*
    * memcpy is disabled, can be enabled with:
    * ti,edma-memcpy-channels = <20 21>;
    * for example. Note that these channels need to be
    * masked in the xbar as well.
    */
    };


    gpmc: gpmc@50000000 {
    compatible = "ti,am3352-gpmc";
    ti,hwmods = "gpmc";
    reg = <0x50000000 0x37c>; /* device IO registers */
    interrupts = <GIC_SPI 15 IRQ_TYPE_LEVEL_HIGH>;
    dmas = <&edma_xbar 4 0>;
    dma-names = "rxtx";
    gpmc,num-cs = <8>;
    gpmc,num-waitpins = <2>;
    #address-cells = <2>;
    #size-cells = <1>;
    interrupt-controller;
    #interrupt-cells = <2>;
    gpio-controller;
    #gpio-cells = <2>;
    status = "disabled";
    };


    &gpmc{
    depth = <1>; /* only create devices on depth 1 */
    status = "okay";

    #address-cells = <2>;
    #size-cells = <1>;
    pinctrl-names = "default";
    pinctrl-0 = <&gpmc_pins_default>;

    ranges = <0 0 0x01000000 0x01000000>; /* CSn0 0, addr 0x01000000, size 0x1000000 (16MiB) */
    gpmc_device0@0,0 {
    compatible = "cfi-flash";
    linux,mtd-name= "intel,pf48f6000m0y1be";
    status = "okay";
    reg = <0 0 0x01000000>;

    /* CONFIG 1 */
    gpmc,sync-read = <1>;
    gpmc,sync-write = <1>;
    bank-width = <2>; /* GPMC_CONFIG1_DEVICESIZE(1) 2: 16bits */
    gpmc,mux-add-data = <0>; /* GPMC_CONFIG1_MUXTYPE(0) 2: address-data multiplexing mode */
    gpmc,burst-length = <16>; /** 16 **/
    gpmc,burst-read = <1>;
    gpmc,burst-write = <1>;
    gpmc,clk-activation-ns = <5>; /* GPMC 信号相对于 FCLK 到来的延时时间 */

    /* CONFIG 2 */
    gpmc,sync-clk-ps = <7500>; /**15000**/ /*9615 14000 15000*/
    gpmc,cs-on-ns = <5>; /**15 0 **/
    gpmc,cs-rd-off-ns = <60>; /** 108 **/ /*101*/
    gpmc,cs-wr-off-ns = <60>; /*101*/

    /* CONFIG 3 */
    gpmc,adv-on-ns = <0>; /** 3 **/ /*0*/ /* control an address and byte-enable valid setup time */
    gpmc,adv-rd-off-ns = <9>; /** 21 **/ /*12*/ /* control an address and byte-enable valid hold time */
    gpmc,adv-wr-off-ns = <9>; /** 21 **/ /*12*/ /* control an address and byte-enable valid hold time */

    // /* CONFIG 4 */
    gpmc,oe-on-ns = <9>; /** 34 **/ /** MAX = 56ns depend on start get data time **/
    gpmc,oe-off-ns = <55>; /** 98 **/
    gpmc,we-on-ns = <9>; /*27*/
    gpmc,we-off-ns = <55>;

    /* CONFIG 5 */
    gpmc,rd-cycle-ns = <60>; /*101*/
    gpmc,wr-cycle-ns = <60>; /*101*/
    gpmc,access-ns = <40>; //读数据开始时间
    gpmc,page-burst-access-ns = <7>; //读一个数据的时间

    /* CONFIG 6 */
    gpmc,bus-turnaround-ns = <0>; /* between two large different access deley time */
    gpmc,cycle2cycle-delay-ns = <0>; /**0**/
    gpmc,wr-data-mux-bus-ns = <0>;
    gpmc,wr-access-ns = <50>; /*95*/

    gpmc,cycle2cycle-samecsen;
    gpmc,cycle2cycle-diffcsen;
    };