This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6745 SPI配置SPI时钟为10Mhz时,无法连续发送数据



C6745  SPI配置SPI时钟为10Mhz时,无法连续发送数据。波形如下,当SCK发送两个字节后,就会有1.13us的SCK高电平出现。

查阅了一下手册,和这个延时相关的是SPIDAT1寄存器的WDEL bit 和 SPIFMTn寄存器的WDELAY  bit。
实际我们设置的WDEL bit = 0 , WDELAY  bit = 0。