采用的是论坛提供的 K1 STK v1.1 例程 进行自循环测试 得到的结果如下。显示的是传输成功,但是我在memory browser中分别查看 地址0xc002000和地址0x1080a200的数据 分别为00000027和00000034.很明显数据不对啊,但是completion code=0 说明传输正确啊。这是怎么回事儿呢??
SWRITE from 0x c002000 to 0x1080a200, 8 bytes, 736 cycles, 86 Mbps, completion code = 0
SWRITE from 0x c002000 to 0x1080a200, 16 bytes, 688 cycles, 186 Mbps, completion code = 0
SWRITE from 0x c002000 to 0x1080a200, 32 bytes, 688 cycles, 372 Mbps, completion code = 0
SWRITE from 0x c002000 to 0x1080a200, 64 bytes, 689 cycles, 743 Mbps, completion code = 0
SWRITE from 0x c002000 to 0x1080a200, 128 bytes, 812 cycles, 1261 Mbps, completion code = 0
SWRITE from 0x c002000 to 0x1080a200, 256 bytes, 1077 cycles, 1901 Mbps, completion code = 0