This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66AK2H12的SRIO loopback如果选择serdes模式,就跑不下去,但是digital的loopback跑下来是没问题的



TI专家,你好

    我们根据K2H的开发板开发了自己的板子,现在跑srio的serdes loopback模式的时候会卡住,但是跑digital的loopback是没问题的,测了时钟156.25MHz是有的,是哪里配置不对吗?

   测试例程是K2_STK_DSP_v1.1里的,就改了loopback模式,SRIO_Loopback_Mode loopback_mode= SRIO_SERDES_LOOPBACK;

   请问其他还要改吗?

JTAG ID= 0x2b98102f. This is a K2H/K2K device, version variant = 2
DEVSTAT= 0x02003671. little endian, no boot or I2C slave boot, boot master is ARM core, PLL configuration implies the input clock for core is 100MHz
SmartReflex VID= 47, required core voltage= 1.001V.
Die ID= 0x0a009001, 0x0c0003b4, 0x40000000, 0x4ff80000
DSP speed grade = 800MHz, ARM speed grade= 800MHz
Initialize main core clock = 122.88MHz/4x39 = 1198MHz
K2H DDR3A initialization
Initialize DDR data rate = 100.000/1*20/6*4= 1333.3 MTS, bus width = 64 bits.
DDR PHY status PGSR0=0xb0000fff.
SRIO_SERDES_LOOPBACK test start............................................
Enable Exception handling...
SRIO link speed is 5.000Gbps
SRIO path configuration 4xLaneABCD     

  • 请看一下KeyStone_2_SRIO_STK_User's_Guide,下面是否有配置?
    The Loopback field [22:21] in SRIO SERDES Transmit Channel Configuration Registers and Loopback field [24:23] in SRIO SERDES Receive Channel Configuration Registers are used to enable the SERDES loopback test. Following code shows the configuration:
    serdesRegs->link[i].CFGRX |=
    (serdes_cfg->linkSetup[i]->loopBack<<SERDES_RX_CFG_LOOPBACK_SHIFT)|

    serdesRegs->link[i].CFGTX |=
    (serdes_cfg->linkSetup[i]->loopBack<<SERDES_TX_CFG_LOOPBACK_SHIFT)|
  • Hi Shine,

    在csl_serdes_srio.h有做以下定义,这个应该就是跟KeyStone_2_SRIO_STK_User's_Guide的serdes loopbakc配置匹配的地方,但是这里面的寄存器配置跟KeyStone Architecture  SRIO User Guide.pdf这个手册对不上啊,包括SRIO配置寄存器的基地址和偏移地址以及每位的定义,请问keystone2的SRIO有更新的文档吗?

       if (loopback_mode == CSL_SERDES_LOOPBACK_ENABLED)

       {

       CSL_FINSR(*(volatile uint32_t *)(base_addr + 0x200*(lane_num+1)),31,24, 0x40);

       }

    上面这个函数是往24~31位写0x40,但是手册里面确是RX CFG的23~24/TX CFG的21~22写11,寄存器偏移地址也对不上。

  • 我把您的问题发到e2e上了,请关注下面的帖子。
    e2e.ti.com/.../973523