This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678之间网络测试



各位专家大神,请教一下:

我利用K1_STK_v1.1文件中的GE工程测试两个C6678之间的网络,两个DSP分别是通过SGMII0和SGMII1相连的,我修改工程中的

GE_Test_Data_Path test_data_path= GE_TEST_DSP0_TO_DSP1;

port口对应每个DSP相连的port口

GE_Port_Connection port_connect[GE_NUM_ETHERNET_PORT]=
{
GE_PORT_SGMII_CONNECT,//SGMII port 0
GE_PORT_NOT_USED//SGMII port 1
};

两个DSP间链路可以通信,但是用SGMII0连接的DSP在接收到26包之后中断interrupt void GE_Message_ISR()就一直无法触发了,但是这个DSP网对端发送数据对端是可以收到的,而且有问题的这个DSP我试过GE_TEST_SERDES_LOOPBACK这个模式是没有问题的,可以一直循环测试。

请问这个可能是什么问题?