高32位在前 低三十二位在后 第二个351按理论应进位为352
读count值的操作如下

进位产生的突变

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请详细描述一下您的timer配置,如64bit timer时用到了哪个timer,配置成了什么mode? 32bit timer时用到了哪个timer,配置成了什么mode? 单独的32bit timer可以正常运行吗?
32bit单独使用正常 具体不知道您说的是模式指什么 下面我将把所欲关于两个定时器的操作以贴图放上来
64bit 配置是timer_test.c 中包含的test_gp_timer 用的是TIMR0 配置如下

Int32 test_gp_timer (Uint8 IntcInstance)
{
/* Clear local data structures */
memset(&TmrObj, 0, sizeof(CSL_TmrObj));
// printf("Debug: Testing 64bit Timer in Single Shot Mode...\n");
/**************************************************************
********************** INTC related code *********************
**************************************************************/
/* Open INTC */
vectId = CSL_INTC_VECTID_12;
tmrIntcHandle = CSL_intcOpen(&tmrIntcObj, CSL_GEM_TINTLN, &vectId, NULL);
/* Bind ISR to Interrupt */
EventRecord.handler = (CSL_IntcEventHandler)&TimerInterruptHandler0;
EventRecord.arg = (void *)CSL_GEM_TINTLN;
CSL_intcPlugEventHandler(tmrIntcHandle, &EventRecord);
/* Event Enable */
CSL_intcHwControl(tmrIntcHandle, CSL_INTC_CMD_EVTENABLE, NULL);
/**************************************************************
********************** Timer related code ********************
**************************************************************/
/* Open the timer. */
hTmr = CSL_tmrOpen(&TmrObj, IntcInstance, NULL, &status);
if (hTmr == NULL)
return -1;
/* Set the timer mode to 64bit GP Timer Mode and set the PRD registers */
hwSetup.tmrTimerMode = CSL_TMR_TIMMODE_GPT;
hwSetup.tmrTimerPeriodLo = 0xFFFFFFFF; //16998406000
hwSetup.tmrTimerPeriodHi = 0xF0000003;
CSL_tmrHwSetup(hTmr, &hwSetup);
/* Reset the timer ISR Counter. */
timerISRCounter0 = 0;
/* Reset the Timer */
CSL_tmrHwControl(hTmr, CSL_TMR_CMD_RESET64, NULL);
/* Start the timer in SINGLE SHOT Mode. */
CSL_tmrHwControl(hTmr, CSL_TMR_CMD_START64, (void *)&TimeCountMode);
return 0;
}
32bit用的是TIMER2 默认配置的来 具体如下
Int32 test_32bit_timer (Uint32 *LoadValue) {
/**************************************************************
********************** 初始化Timer1 *********************
**************************************************************/
/* Clear local data structures */
memset(&TmrObj1, 0, sizeof(CSL_TmrObj));
/**************************************************************
********************** INTC related code *********************
**************************************************************/
/* Open INTC */
vectId1 = CSL_INTC_VECTID_5;
tmrIntcHandle1 = CSL_intcOpen(&tmrIntcObj1, CSL_GEM_TINT2L, &vectId1, NULL);
/* Bind ISR to Interrupt */
EventRecord1.handler = (CSL_IntcEventHandler)&TimerInterruptHandler1;
EventRecord1.arg = (void *)CSL_GEM_TINT2L;
CSL_intcPlugEventHandler(tmrIntcHandle1, &EventRecord1);
/* Event Enable */
CSL_intcHwControl(tmrIntcHandle1, CSL_INTC_CMD_EVTENABLE, NULL);
/**************************************************************
********************** Timer related code ********************
**************************************************************/
/* Open the timer. */
hTmr1 = CSL_tmrOpen(&TmrObj1, CSL_TMR_2, NULL, &status1);
/* Open the timer with the defaults. */
CSL_tmrHwSetup(hTmr1, &hwSetup1);
/* Stop the Timer */
CSL_tmrHwControl(hTmr1, CSL_TMR_CMD_RESET_TIMLO, NULL);
/* Set the timer mode to unchained dual mode */
hwSetup1.tmrTimerMode = CSL_TMR_TIMMODE_DUAL_UNCHAINED;
CSL_tmrHwSetup(hTmr1, &hwSetup1);
/* Reset the timer ISR Counter. */
timerISRCounter1 = 0;
/* Load the period register */
status1 = CSL_tmrHwControl(hTmr1, CSL_TMR_CMD_LOAD_PRDLO, (void *)LoadValue);
CSL_tmrHwControl(hTmr1, CSL_TMR_CMD_START_TIMLO, (void *)&TimeCountMode1);
return 0;
}