例程12b,当USER_MOTOR_RES_EST_CURRENT电流设置的偏小的时候,Rs在线转子位置和编码器对齐的时候就会偶尔出现异常,电机跑飞或者堵转。USER_MOTOR_RES_EST_CURRENT的数据设置的大一点空载就正常了,文档建议值是额定电流的10%-20%。当我的负载很大的时候,10%-20%的额定电流不能给使电机动作的时候,这个时候还会存在转子位置校准不对的,这个时候应该怎么处理呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
例程12b,当USER_MOTOR_RES_EST_CURRENT电流设置的偏小的时候,Rs在线转子位置和编码器对齐的时候就会偶尔出现异常,电机跑飞或者堵转。USER_MOTOR_RES_EST_CURRENT的数据设置的大一点空载就正常了,文档建议值是额定电流的10%-20%。当我的负载很大的时候,10%-20%的额定电流不能给使电机动作的时候,这个时候还会存在转子位置校准不对的,这个时候应该怎么处理呢?
好的,我将你的问题升级至英文E2E了,由于国外时差原因,可能要今晚才能回复,还请耐心等待
e2e.ti.com/.../boostxl-drv8305evm-problem-of-parameter-setting-user_motor_res_est_current
嗯,看了回复了,和我的问题有点区别吧。我希望知道的是负载重的时候怎么保证Rs校准转子位置的稳定性。文档的Rs校准电流是额定的10%-20%,如果我把校准电流调到额定电流,是否有什么隐患。调到额定电流可以用,担心是否有隐患。例程12B,通过Rs校准编码器的偏移角度。