This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSEVM572X: TIDL部分的Insufficient OpenCL global memory问题

Part Number: TMDSEVM572X


硬件:TMDSEVM572X

软件:Processor SDK Linux 06_03_00_106

问题:无法调整OpenCL的global memory

按照Sizing device side heaps,在程序中设置好相关PARAM_HEAP_SIZE和NETWORK_HEAP_SIZE,发现NETWORK_HEAP_SIZE依然未满足要求。

于是按照Insufficient OpenCL global memory进行以下操作:

(1)把prebuilt_image文件夹的am57xx-evm-reva3.dtb转换成am57xx-evm-reva3.dts

(2)修改am57xx-evm-reva3.dts文件,

          a) cmem_block_mem@a0000000部分,“reg = <0x0 0xa0000000 0x0 0xc000000>;”改为“reg = <0x0 0xa0000000 0x0 0x18000000>;”,“phandle”部分改为“linux,phandle = <0x13c>;”

          b) cmem_block@0部分,“memory-region”部分改为“memory-region = <0x13c>;”,“cmem-buf-pools = <0x1 0x0 0xc000000>;”改为“cmem-buf-pools = <0x1 0x0 0x18000000>;”,其他删去

(3)dts文件转为dtb文件后复制回/boot,重启

注:把dts文件转回dtb文件有附图报错,我是加了-f参数,强行转换的。推测与此有关,dts文件没有正确配置好。

再次运行程序,报同样错误。程序报错:

谢谢帮助!

  • 我咨询相关工程师后再给您回复。

  • 你好。

    我今天只对dts文件做以下修改:

    (1)cmem_block_mem@a0000000部分,“reg = <0x0 0xa0000000 0x0 0xc000000>;”改为“reg = <0x0 0xa0000000 0x0 0x18000000>;”

    (2)cmem_block@0部分,“cmem-buf-pools = <0x1 0x0 0xc000000>;”改为“cmem-buf-pools = <0x1 0x0 0x18000000>;”

    dts文件转换dtb文件无报错,但是当我重启设备后,CMEM大小依旧没有变化。希望得到对应解决方案。

    谢谢!

  • 请将您目前设备树中memory部分的配置直接贴上来,谢谢!

  • memory@0 {
    		device_type = "memory";
    		reg = <0x0 0x80000000 0x0 0x80000000>;
    	};
    
    	reserved-memory {
    		#address-cells = <0x2>;
    		#size-cells = <0x2>;
    		ranges;
    
    		ipu2-memory@95800000 {
    			compatible = "shared-dma-pool";
    			reg = <0x0 0x95800000 0x0 0x3800000>;
    			reusable;
    			status = "okay";
    			phandle = <0xa0>;
    		};
    
    		dsp1-memory@99000000 {
    			compatible = "shared-dma-pool";
    			reg = <0x0 0x99000000 0x0 0x4000000>;
    			reusable;
    			status = "okay";
    			phandle = <0xa6>;
    		};
    
    		ipu1-memory@9d000000 {
    			compatible = "shared-dma-pool";
    			reg = <0x0 0x9d000000 0x0 0x2000000>;
    			status = "okay";
    			no-map;
    			phandle = <0x99>;
    		};
    
    		dsp2-memory@9f000000 {
    			compatible = "shared-dma-pool";
    			reg = <0x0 0x9f000000 0x0 0x800000>;
    			reusable;
    			status = "okay";
    			phandle = <0xda>;
    		};
    
    		mmu-early-page-tables@95700000 {
    			reg = <0x0 0x95700000 0x0 0x100000>;
    			no-map;
    		};
    
    		cmem_block_mem@a0000000 {
    			reg = <0x0 0xa0000000 0x0 0x18000000>;
    			no-map;
    			status = "okay";
    			phandle = <0xed>;
    		};
    
    		cmem_block_mem@40500000 {
    			reg = <0x0 0x40500000 0x0 0x100000>;
    			no-map;
    			status = "okay";
    			phandle = <0xee>;
    		};
    	};

    以上修改了cmem_block_mem@a0000000部分。只修改了reg语句。

    	cmem {
    		compatible = "ti,cmem";
    		#address-cells = <0x1>;
    		#size-cells = <0x0>;
    		#pool-size-cells = <0x2>;
    		status = "okay";
    
    		cmem_block@0 {
    			reg = <0x0>;
    			memory-region = <0xed>;
    			cmem-buf-pools = <0x1 0x0 0x18000000>;
    			phandle = <0x211>;
    		};
    
    		cmem_block@1 {
    			reg = <0x1>;
    			memory-region = <0xee>;
    			phandle = <0x212>;
    		};
    	};

    以上修改了cmem_block@0部分。只修改了cmem-buf-pools语句。

    仅修改以上两个语句,则am57xx-evm.dts和am57xx-evm-reva3.dts都可顺利转换为dtb文件。