Other Parts Discussed in Thread: OMAP-L138
我使用的芯片本是OMAPL138EZWTD4E,也不想使用这个芯片的加密功能,只想当做普通的138芯片使用。
目前已经可以解锁芯片的JTAG了,但是还没有找到工具软件,可以实现把AIS文件烧写到NAND里。
请问有没有可用的工具软件或方法,可以把AIS文件烧写到NAND里,以便可以自动上电启动。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我使用的芯片本是OMAPL138EZWTD4E,也不想使用这个芯片的加密功能,只想当做普通的138芯片使用。
目前已经可以解锁芯片的JTAG了,但是还没有找到工具软件,可以实现把AIS文件烧写到NAND里。
请问有没有可用的工具软件或方法,可以把AIS文件烧写到NAND里,以便可以自动上电启动。
请到下面的网站下载软件包,里面有SecureHexAIS_OMAP-L138.exe可以转换成.
http://software-dl.ti.com/dsps/dsps_public_sw/omap_l1x/omapl13x_c674x_generic_secure/latest/index_FDS.html
烧写工具和非加密的一样。
The examples and utilities discussed in this application report can be downloaded from the following URL:
https://www.ti.com/lit/an/spracm8a/spracm8a.pdf
我尝试使用串口烧写工具 ,但是失败,显示信息如下:
sfh_OMAP-L138.exe -flash_noubl -flashType NAND -p COM6 u-boot.bin
-----------------------------------------------------
TI Serial Flasher Host Program for OMAP-L138
(C) 2012, Texas Instruments, Inc.
Ver. 1.67
-----------------------------------------------------
[TYPE] Single boot image
[BOOT IMAGE] u-boot.bin
[TARGET] OMAPL138
[DEVICE] NAND
[NAND Block] 1
Attempting to connect to device COM6...
Press any key to end this program at any time.
(AIS Parse): Read magic word 0x41504954.
(AIS Parse): Waiting for BOOTME... (power on or reset target now)
(AIS Parse): BOOTME received!
(AIS Parse): Performing Start-Word Sync...
(AIS Parse): Performing Ping Opcode Sync...
(AIS Parse): Processing command 0: 0x58535901.
(AIS Parse): Performing Opcode Sync...
(Serial Port): Read error! (操作已超时。)
(AIS Parse): I/O Error in read!
(Serial Port): Read error! (操作已超时。)
(AIS Parse): I/O Error in read!
如果您的板子和TI EVM板不一样的话,需要做相应的修改,请参考下面的文档2.3 Modifications for Custom Boards。
https://www.ti.com/lit/an/spracm8a/spracm8a.pdf
修改后,按照下面的步骤重新编译flashwriter.
https://e2echina.ti.com/support/processors/f/processors-forum/196294/faq-faq